Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Example Programs for the Keysight N5700 Family of DC Power Supplies

This self-executing zip file contains an example program for the Keysight N5700 DC Power Supplies. To download, click on the link below and either run the program from its current location or save it to a hard drive. Execute the program. The installation directory defaults to C:\Program Files\Keysight\N5700 or the user can specify the directory to install the sample programs.

This file contains an example in the following program languages with the following IO libraries:

  • C++ with VISA
  • Microsoft Visual C++ 6.0 with VISA
  • Microsoft Visual Basic 6.0 with VISA and VISA-COM
  • Microsoft Excel with VISA
  • Keysight VEE with Direct I/O

The sample program is called EZSample. This is a simple example that sets voltage, current, and the protection features of the N5700 Power Supplies. It also measures voltage. This is a perfect introduction to programming the N5700 DC Power Supplies.

Documents & Downloads

N5700 Series System DC Power Supplies Example Programs 
Example programs for the N5741-49A, N5750-52A, N5761-69A, N5770-72A power supplies.

Programming Example 2004-09-01