Contact an Expert

Cellular videos - MIMO Videos

Keysight engineers are experts in test and focus on developing equipment and systems ahead of the technology wave. View these videos below to learn more about the intricacies of wireless from Keysight, and much more.

Accelerate Wireless Design and Test with Flexible, High-Performance Platforms

How to accelerate RF device testing

Keysight PXI Modular RF Test Solutions 

To accelerate RF device testing, Keysight offers state-of-the-art solutions for the wireless industry that ease business pressures—reduce technical difficulties—increase test confidence—and lower test costs. All while preparing for the future, too. So you're ready for the demands of RF device testing today...and tomorrow. The Keysight PXI Modular RF Test Solution provides a comprehensive suite of hardware and software that work seamlessly together.

29 September 2013

Keysight's new 8x8 MIMO simulation and measurement capabilities

8x8 LTE MIMO Analysis | N7109A Signal Analyzer | 89600 VSA | SystemVue 

See how Keysight's new 8x8 MIMO simulation and measurement capabilities help LTE basestation designers stay ahead of rapidly evolving LTE standards test requirements. This video demonstrates 8x8 MIMO simulation, signal creation, and troubleshooting measurements using new features in SystemVue, 89600 VSA software, X-Series Signal Generators, and N7109A Multi-channel Signal Analyzer

January 8, 2013

Addressing VHT 80211ac WLAN MIMO Design Test Challenges

Addressing VHT 802.11ac WLAN MIMO Design and Test Challenges  

Demonstration on how to create and analyze a very high throughput 160 MHz 802.11ac WLAN two channel MIMO signal using integrated design and test equipment. SystemVue and 89600 VSA software are used early in the design phase for 802.11ac system design to evaluate design trade-offs. And, then for hardware testing they are combined with 81180A AWGs, MXG signal generators, and a high performance multichannel Infiniium oscilloscope or PXI vector signal analyzer to perform 802.11ac MIMO measurements on DUT hardware.

May 31, 2012

Demonstration of testing the MIMO OTA performance of an LTE device

MIMO OTA Two-Stage Method Using PXT and PXB

This video is a demonstration of testing the MIMO OTA performance of an LTE device using the two-stage method with Keysight Technologies' N5106A PXB and E6621A PXT. This method is efficient and cost-effective and can be used for multiple stages of test including design verification testing of antennas or devices on a lab bench. 3GPP and CTIA are currently evaluating this method to be added to LTE conformance testing.

March 5, 2012

Keysight LTE Video N7100 MIMO LTE

Demonstration of analysis of un-impaired and impaired LTE MIMO signal

This video contains an analysis of a 2x2 LTE MIMO signals using the N7100 Multi-channel Signal Analysis Platform and the 89600 Vector Analysis Software. Both an unimpaired signal and signal impaired by static fading are examined.

22 Feb 2011

LTE Video N7100 MIMO WiMax Keysight

Demonstration of analysis of un-impaired and impaired WiMAX(TM) MIMO signal

This video contains an analysis of a 2x2 WiMAXTM MIMO signals using the N7100 Multi-channel Signal Analysis Platform and the 89600 Vector Analysis Software. Both an un-impaired signal and signal impaired by pedestrian fading are examined.
 

WiMAX is a trademark of the WiMAX Forum.

22 Feb 2011

N7100 MIMO WiFi Keysight

Demonstration of analysis of an un-impaired MIMO WiFi signal

This video demonstrates how Keysight’s N7100 Multichannel signal analysis platform can identify and troubleshoot problems in a WiFi signal.

22 Feb 2011

Video N7100 MIMO Benefits Keysight

N7100 Multi-channel Signal Analysis support of MIMO development

The N7100 Multi-channel analysis platform helps solve difficult problems in MIMO development. The video is an overview of the many measurement and analysis capabilities of the N7100.

22 Feb 2011

Long Term Evolution (LTE) - demonstration of an end-to-end test of the Xilinx LTE eNB MIMO baseband receiver that has been implemented on the ML605 Virtex 6 development board

LTE eNB MU-MIMO Receiver Baseband Testing

This is a demonstration of an end-to-end test of the Xilinx LTE eNB MIMO baseband receiver that has been implemented on the ML605 Virtex 6 development board, using signals created in Keysight SystemVue and output through the Keysight N5106A PXB baseband generator and channel emulator, and the N5102A Digital Signal Interface Module (DSIM). The digital lines are physically connected to the ML605 using an adapter card to the VITA 57 FMC connector.

16 April 2010

Long Term Evolution (LTE) - demonstration of a 2x2 LTE MIMO system configuration where the Keysight 89600 VSA software and Keysight N9020A MXA signal analyzers are used to make an LTE MIMO composite EVM measurement

LTE MIMO Composite EVM

This is a demonstration of a 2x2 LTE MIMO system configuration where the Keysight 89600 VSA software and Keysight N9020A MXA signal analyzers are used to make an LTE MIMO composite EVM measurement on signals from the Keysight N5182A MXG signal generators.

13 Jan 2010

Long Term Evolution (LTE) - demonstration of how Keysight SystemVue 2009 is used for FPGA prototype verification for TDD-LTE MIMO systems

4G MIMO LTE Antenna and PCB Design using SystemVue 2009

A demonstration of how Keysight SystemVue 2009 is used for FPGA prototype verification for TDD-LTE MIMO systems.

11 Jan 2010

Here are other sites to keep you current on the products, industry and applications, and where to get the latest application notes, CDs, posters, and more.

  • Learn more about 3GPP LTE Order LTE Application Notes, CDs, posters and Keysight’s LTE book.
  • Long Term Evolution - LTE Test LTE test and design resources from Keysight. Learn about LTE Test Equipment from design automation to network deployment.
  • MIMO Test Multiple Input, Multiple Output antenna technology as implemented in LTE, WiMAX™ and WLAN 802.11n testing resources from Keysight
  • 4G LTE Advanced Test Keysight 4G LTE Advanced design and test products for early 4G development. Addressing basic to advanced LTE 4G test challenges, technology and deployment. 

See the full collection of Cellular Videos, including LTE, LTE-A, MIMO, HSPA, MSR and MIPI.

To see the complete Cellular video collection see our YouTube channel http://www.youtube.com/user/agilentcellular 

Here are other sites to keep you current on the products, industry and applications, and where to get the latest application notes, CDs, posters, and more.