Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Cellular videos - LTE Videos

Keysight engineers are experts in test and focus on developing equipment and systems ahead of the technology wave. View these videos below to learn more about the intricacies of wireless from Keysight, and much more.

Accelerate Wireless Design and Test with Flexible, High-Performance Platforms

Video - The end-to-end IP Data Throughput demonstration illustrates how to measure IP data performance at sustained

End-to-End IP Data Throughput, With/Without Channel Impairments, Using E7515A UXM Wireless Test Set  

UXM Videos demonstrate complex LTE-Advanced measurements performed with relative ease. The end-to-end IP Data Throughput demonstration illustrates how to measure IP data performance at sustained, maximum data-rates with UXM to assess device performance in real world conditions.

12 Feb 2014

The DL Channel Configuration Flexibility video illustrates how to test UEs with myriad LTE resource allocations

DL Channel Configuration Flexibility for LTE Receiver Testing Using the E7515A UXM Wireless Test Set 

UXM Videos demonstrate complex LTE-Advanced measurements performed with relative ease. The DL Channel Configuration Flexibility video illustrates how to test UEs with myriad LTE resource allocations, and measure performance in real world conditions using the UXM wireless test set.

12 Feb 2014

The CSI video illustrates how to measure device performance by ensuring the UE correctly reports CSI

How to Perform CSI Measurements Using the E7515A UXM Wireless Test Set 

UXM Videos demonstrate complex LTE-Advanced measurements performed with relative ease. The CSI video illustrates how to measure device performance by ensuring the UE correctly reports CSI (CQI, PMI or RI) in real world conditions using the UXM wireless test set.

12 Feb 2014

Video - LTE-A Carrier Aggregation Technology and Test Challenges

LTE-A Carrier Aggregation technology and test challenges 

LTE-A carrier aggregation device test performed under real world conditions represents a challenge. The answer lies in an integrated functional and RF test solution for Category 4/6 device test with MIMO, fading and noise generation.

28 Jan 2014

Learn the latest LTE and LTE-Advanced expert and 3GPP representative Moray Rumney on the current work on Release 12 for LTE-Advanced

LTE and LTE-Advanced Expert Moray Rumney 

Learn the latest from Keysight’s LTE and LTE-Advanced expert and 3GPP representative Moray Rumney on the current work on Release 12 for LTE-Advanced. This video will review the new focus areas for Release 12 and current work being done.

5 Jan 2014

Video Increase Power Amplifier Efficiency | Envelope Tracking | Signal Studio Software

Increase Power Amplifier Efficiency | Envelope Tracking | Signal Studio Software 

Desc: Get more out of your mobile power amplifier with envelope tracking, a new technique used to increase power amplifier efficiency. Watch this video to see how to increase power amplifier efficiency by increasing the power supply voltage of the power amplifier, making the input signal larger, and decreasing the power supply voltage when the input signal is lower.

Oct 18, 2013
 

Video Demo - Verifying LTE device behavior

Test the Link Between LTE Base Stations & User Equipment  

LTE signals are very complex and communications between the base station and the user equipment can be difficult to verify. In a closed loop system, it can be hard to pinpoint where a signal problem originates. The Keysight 89600 VSA software can test the link between the LTE base station and user equipment and the comprehensive set of LTE physical layer tools, along with the 89600 WLA software for wireless link analysis, allow for decoding of higher layer LTE messages. Watch this video to learn more about verifying LTE device behavior.

July 3, 2013

LTE eNB Receiver Testing | N7649B Test Case Manager

LTE eNB Receiver Testing | N7649B Test Case Manager  

It is not easy task to ensure compliance with the mandated signal levels and LTE signal requirements as defined by the 3GPP standard for testing LTE eNB receivers. Watch this video to see how the Keysight Test Case Manager software automatically configures the wanted and interfering signals as required for the TS36.141 Receiver Characteristics tests for use with your Keysight signal generator. Additionally, flexible control of system parameters enables customization and the unique SCPI log viewer makes it easy to automate the 3GPP tests.

January 30, 2013

LTE and Evolution to 4G Wireless Book 2nd Edition - Keysight

LTE and the Evolution to 4G Wireless Second Edition  

From both a technical and a practical point of view, there is still much to examine, evaluate and understand in 3GPP LTE cellular technology and the evolution to LTE-Advanced. The first edition of this book, with content from Keysight engineers and other industry experts, covered basic concepts such as OFDMA, MIMO and SC-FDMA. This second edition, with over 42 authors, is updated to the latest 3GPP standards, June 2012 and Release 11, and looks forward to Release 12.

Feb 1 , 2013

Demo by Keysight - how to debug and validate the vector signal path in LTE radio

LTE Digital and Analog Vector Modulation Debug

Watch this video to learn how to debug and validate the vector signal path in an LTE radio. A common analysis environment allows for both digital and analog/RF teams to evaluate the quality of key LTE signals. Both digital and analog signals are processed by the 89600 Vector Signal Analyzer (VSA) software where the constellation diagram, spectral content, and error vector magnitude can be observed and compared to SystemVue simulation results.

March 27, 2012

89600 WLA software Keysight

89600 WLA software - LTE link analysis

This video demonstrates how to utilize 89600 WLA software (89620B or 89620BN) to verify the UE uplink configuration and uncover unexpected activity in the operation of the HARQ control loop.

March 5, 2012

N7100 Multi-Channel Signal Analyzer + 89600 VSA Software TD-LTE Beamforming MIMO 8-channel measurement solution

Verify and Visualize your TD-LTE Beamforming Signals

Watch as a Keysight engineer introduces the Keysight N7100 Multi-Channel Signal Analyzer + 89600 VSA Software TD-LTE Beamforming MIMO 8-channel measurement solution. This solution from Keysight provides an 8-channel phase coherent measurement solution to enable verification and visualization of TD-LTE base station RF antenna beamforming signals.

January 30, 2012

ACPR measurement video

Fast adjacent channel power ratio (ACPR) measurements with Keysight's N9030A PXA signal analyzer 

Watch as a Keysight engineer makes a measurement using the Keysight PXA signal analyzer's fast ACPR measurement. This video shows how a correctly set up PXA can make a measurement in 10 ms (including data transfer time), while exhibiting better than the specified -81 dBc dynamic range. The PXA's fast ACP mode is optimized for throughput. For the highest dynamic range, the PXA has an integrated bandwidth method, which has nominally better -88 dBc W-CDMA ACLR dynamic range (with noise correction on).

Sept 15, 2011

 

LTE EVM measurements on Keysight's high performance N9030A PXA signal analyzer 

Watch as a Keysight engineer makes a low EVM measurement using the Keysight PXA signal analyzer's LTE measurement application. This video shows how a correctly set up PXA can achieve low residual EVM measurements for an uplink signal.

Sept 15 2011

N9030A PXA signal analyzer

One-button third order intercept measurements with Keysight's N9030A PXA signal analyzer 

Watch as a Keysight engineer makes a TOI measurement using the Keysight PXA signal analyzer's one-button measurement capability. This video shows how a correctly set up PXA with appropriate attenuation can easily make high dynamic range measurements.

Sept 15, 2011

 

Demonstration of VoIP with a 4G LTE USB Modem

This video demonstrates the use of the Keysight E6621 PXT Wireless Communications Test Set with VoIP with a 4G LTE (LTE-Advanced) USB modem.

May 2, 2011

 Demonstrates how to accelerate time-to-market for LTE UE designs

Demonstration of Handovers between LTE and eHRPD Cells (Inter-RAT)

This video demonstrates how to accelerate time-to-market for LTE UE designs with handovers between LTE and eHRPD Cells (Inter-RAT) using the Keysight E6621 PXT.

May 2, 2011

Battery Drain Video: Seamless Measurement Ranging on the N6781A

This is a demonstration of seamless measurement ranging, allowing engineers to view their entire current waveform, from nA to A, in one pass and in one picture, utilizing the features of the Keysight N6781A SMU and N6705B DC Power Analyzer.

6 July 2010

Long Term Evolution (LTE) eNB Closed-loop Conformance Testing

LTE eNB Closed-loop Conformance Testing

This is a demonstration of how the Keysight N5106A PXB baseband generator and channel emulator, N7624B Signal Studio for LTE software, and N5182A MXG signal generator are configured for eNB closed-loop conformance test. Specifically showing how the equipment responds to required feedback from an eNB for the uplink timing adjustment test.

12 Jan 2010

Long Term Evolution (LTE) demonstration of an overview and detailed analysis of an LTE downlink signal using the Keysight 89600 VSA software

LTE 5MHz Downlink signal  

This is a demonstration of an overview and detailed analysis of an LTE downlink signal using the Keysight 89600 VSA software.

11 Nov 2009

Long Term Evolution (LTE) - demonstration of an EVM and uncoded BER measurement using the Keysight ADS, N9020A MXA signal analyzer, and N5182A MXG signal generator

LTE EVM and BER Measurement Using a Connected Solutions Equipment Configuration 

LTE Connected Solutions demonstration of an EVM and uncoded BER measurement using the Keysight ADS, N9020A MXA signal analyzer, and N5182A MXG signal generator.

24 July 2008

Here are other sites to keep you current on the products, industry and applications, and where to get the latest application notes, CDs, posters, and more.

  • Learn more about 3GPP LTE Order LTE Application Notes, CDs, posters and Keysight’s LTE book.
  • Long Term Evolution - LTE Test LTE test and design resources from Keysight. Learn about LTE Test Equipment from design automation to network deployment.
  • MIMO Test Multiple Input, Multiple Output antenna technology as implemented in LTE, WiMAX™ and WLAN 802.11n testing resources from Keysight
  • 4G LTE Advanced Test Keysight 4G LTE Advanced design and test products for early 4G development. Addressing basic to advanced LTE 4G test challenges, technology and deployment. 

See the full collection of Cellular videos, including LTE, LTE-A, MIMO, HSPA, MSR and MIPI.

To see the complete Cellular video collection see our YouTube channel https://www.youtube.com/keysightcellular