Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

FieldFox Customer Support - Instrument Console Utility

The Instrument Console utility is intended for experimenting with SCPI commands for the FieldFox.

This utility is not formally supported by Keysight, use "as is."

  1. Download the ic.exe file to your PC and execute it
  2. Use the -a command to connect to your FieldFox. If you have problems establishing the telnet connection click here

This utility can be used with Keysight IO Libraries instead of giving the IP address.

If an error is continuously returned, try increasing the timeout (-t

Info from the help file:

Help info for Instrument Console, updated August 1, 2010. filename: ic_doc.doc

The following is a dump from the help command with some notes added.

IC > ?

Keysight Technologies InstrumentConsole, v0.64

*** THIS SOFTWARE IS UNSUPPORTED ***

*** USE AT YOUR OWN RISK! ***

Command Summary: