Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Can I use Command Expert without an Internet connection?

Yes. If you work in a secure environment without internet access, you can still use Command Expert. Ordinarily, Command Expert uses your Internet connection to download SCPI command sets from the Command Expert Server. But you can configure Command Expert to use a folder on your hard drive as a source of SCPI command sets instead; see the Help Documentation section "Managing Command Sets".

Command Expert 1.2 allows you to set the Command Set Source to “Work Offline”. In this mode Command Expert will not connect to the command set server. You can also select a file path for Command Expert to search for command sets downloaded locally. See the Help Documentation section "Command Set Source" for more details.

Last Revised April 28th, 2013