Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

How long does the system user alignment of my PSA EMI Measurement Receiver take to run?

There are three different softkeys on the internal user alignment menu that will execute the internal alignments. These three softkeys give the user the option of doing either of the two signal path alignments individually or both at the same time. So, the time that the user alignments will take will depend on what is selected. Below is a table with the approximate times for each of these three selections.

User Alignment Times
SoftkeySignal Path AlignedApproximate Time To Complete
Align 9 kHz to 30 MHzConducted1 Minute
Align 30 MHz to 1 GHzRadiated31 Minutes
Align 9 kHz to 1 GHzConducted & Radiated32 Minutes

Documents & Downloads

How often does the system user alignment for the PSA EMI Measurement Receiver need to be run? 
30 days or 3° C temperature change. See contents for details...

FAQ 2012-12-11

Why does my PSA EMI Measurement Receiver tell me that I need to run the user alignment everyday? 
There are a couple of reason why this could be hapening. See FAQ contents for details...

FAQ 2012-03-16

What does the system user alignment of my PSA EMI Measurement Receiver do? 
See contents for details...

FAQ 2012-03-16