Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

When running a Keysight 85876B radiated emission test I accidentally clicked on the 'x' in the upper right corner, and closed the window. How do I restore the window when it has been closed?

To restore the composite trace window, PAUSE the test by clicking 'Pause' button in Test Procedure Execution window - when the flashing red bar appears indicating the test is paused, click 'Start' button to resume the test. The composite trace window should reappear.