您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

How do I create a trigger out signal on the rear of an AC source?

From the front panel:

To generate a SINGLE "Trig OUT", use the following key sequences:

Press [shift] [Output] keys;

Use the function and entry scroll keys to pick {TTLT:STATE "ON"} then press [ENTER] ;

Press [Trigger Control] key;

Use scroll keys to pick {INIT:IMMED} then press [ENTER];

Press [shift] [Trigger] keys.

This initiates a one-time trigger from the Trigger Out BNC connector on the rear panel of the instrument. In order to initiate subsequent triggers, {INIT:IMMED} must first be re-entered each time. Then pressing [shift][Trigger] will initiate a trigger.

To generate a "Trig OUT" each time the [shift][Trigger] is pressed:

Press [shift] [Output] key;

Use the function and entry scroll keys to pick {TTLT:STATE "ON"} then press [ENTER];

Press [Trigger Control] key;

Use scroll keys to pick {INIT:CONT ON} then press [ENTER];

Press [shift] [Trigger] keys.

This initiates a trigger from the Trigger Out BNC connector on the rear panel of the instrument each time [shift] [Trigger] is pushed.

Over the GPIB:

Sample Program

10 OUTPUT 705; "OUTP ON"

20 OUTPUT 705; "OUTP:TTLT ON"

30 OUTPUT 705; "INIT:IMM:NAME TRAN"

40 OUTPUT 705; "TRIG:TRAN:SOUR BUS"

50 OUTPUT 705; "TRIG:IMM"

60 END

相關連結