Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Version 7.x ASAP Best Practices

In an effort to standardize programming practices for the Keysight 5DX, Keysight has created a set of procedures representing 5DX "best practices" that address various aspects of the programming process. These are collectively referred to as the Keysight Supported Application Program (ASAP). These supported application programming practices represent a compilation of inputs from developers and experienced users in the factory and the field. The set of procedures listed here is related to 7.x software releases.

Since ASAP is an integral part of the Test Development process, all ASAP documentation has been built into the new tools and Help System with the 8.x software release.

The ASAP Overview provides a single entry point for all topics that are related to the ASAP method.

If you are using 8.x software releases:

- Refer to the Help System on the 5DX or TDW.

If you are using 7.x software releases:

- Refer to the set of procedures listed below.

Documents & Downloads

ASAP Introduction: READ THIS FIRST 

Application Note 2001-07-26

null PDF 18 KB
CAD Input Formats - Ver 1.1 

Application Note 2001-08-27

null PDF 16 KB
Panelization Procedures - Ver 1.5 

Application Note 2001-08-27

null PDF 27 KB
Selecting an Algorithm Family by Device Type - Ver 1.1 

Application Note 2001-07-26

null PDF 13 KB
Generating Package Data - Ver 1.0 

Application Note 2001-07-26

null PDF 39 KB
Component Subtyping - Ver 1.6 

Application Note 2001-08-27

null PDF 38 KB
View Setup Procedure - Ver 1.5 

Application Note 2001-08-27

null PDF 24 KB
Alignment Setup - Ver 1.4 

Application Note 2001-08-27

null PDF 85 KB
Surface Map Setup - Ver 1.9 

Application Note 2001-08-27

null PDF 177 KB
Surface Map Grid File - Ver. 1.0 
This document contains the initial surface map grid settings for application development. Refer to the ASAP document for Surface Map Setup for proper usage of this file.

Application Note 2001-10-01

null FILE 4 KB
CheckCAD Procedures - Ver 1.6 

Application Note 2001-08-27

null PDF 291 KB
BGA2 Algorithm Setup - Ver 1.3 

Application Note 2001-08-16

null PDF 226 KB
Chip Algorithm Setup - Ver 1.2 

Application Note 2001-07-25

null PDF 85 KB
Connector Algorithm Setup - Ver 1.1 

Application Note 2001-07-26

null PDF 248 KB
FPGullwing Algorithm Setup - Ver 1.3 

Application Note 2001-08-22

null PDF 318 KB
Gullwing Algorithm Setup - Ver 1.3 

Application Note 2001-08-22

null PDF 306 KB
Jlead Algorithm Setup - Ver 1.0 

Application Note 2001-08-27

null PDF 259 KB
PCAP Algorithm Setup - Ver 1.2 

Application Note 2001-10-17

null PDF 583 KB
PTH Algorithm Setup - Ver 1.2 

Application Note 2001-10-17

null PDF 229 KB
RES Algorithm Setup - Ver 1.1 

Application Note 2001-07-26

null PDF 180 KB
Socket Algorithm Setup - Ver 1.0 

Application Note 2001-08-27

null PDF 259 KB
Production Tuning - Ver 1.5 

Application Note 2001-08-27

null PDF 24 KB