Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

What is the Port Reference Impedance Conversion? Is this function available on the ENA / ENA-L?

(SUPPORTED MODELS IN BOLD: E5071C  E5071B/70B  E5070A/71A  E5061A/62A E5061B E5072A)

The Port Reference Impedance Conversion is one of a feature of the Fixture Simulator. This function is only available on the ENA.
Using this function, S-parameter measured with system impedance (50ohm) is converted into S-parameter measured with specific arbitrary impedance.

port reference impedance conversion

 

Converting Port Impedance:

  1. Press the Analysis key, then click Fixture Simulator > Port Z Conversion.
  2. Specify the port reference impedance for the specific
  3. Click Port Z Conversion to change the port impedance conversion function to the ON state.
  4. Click Return.
  5. If Fixture Simulator is OFF, click the key again to enable the Fixture Simulator to the ON condition.