이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

MIMO OTA Two-Stage Method Using PXT and PXB

This video is a demonstration of testing the MIMO OTA performance of an LTE device using the two-stage method with Keysight Technologies' N5106A PXB and E6621A PXT. This method is efficient and cost-effective and can be used for multiple stages of test including design verification testing of antennas or devices on a lab bench. 3GPP and CTIA are currently evaluating this method to be added to LTE conformance testing.

 

본 페이지는 자바스크립트가 허용된 브라우저와 어도비 플래쉬 플레이어가 있어야 정상적으로 보실 수 있습니다.

플래쉬 다운로드 

Learn more about Cellular Videos