이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

How do I remotely read demodulated symbols from the 89601A VSA software using Microsoft Excel?

Disclaimer:
You have a royalty-free right to use, modify, reproduce and distribute the Sample Application Files (and/or any modified version) in any way you find useful, provided that you agree that Keysight Technologies has no warranty, obligations or liability for any Sample Application Files.

Description:
This example demonstrates how to write a Visual Basic for Applications macro in Microsoft Excel to do the following:

  • Take control of a running instance of 89601A or start a new instance
  • Open a recording
  • Setup the software to demodulate an NADC signal
  • Read the RMS EVM, RMS Magnitude error, and RMS Phase error
  • Read the demodulated data symbols
  • Write the error summary data to the Excel spreadsheet

Languages Supported:
Microsoft Excel

Revision Date:
December 29, 2004

Download Instructions:
Save the self extracting archive to disk and open it and click "Unzip" to extract the 89600_Symbol_Table.xls and ACP.sdf files to your C:\temp directory.

Procedure:

  • Open the 89600_Symbol_Table.xls file with Microsoft Excel
  • If prompted to enable or disable macros, select "Enable Macros"
  • Follow the procedure documented in the Spreadsheet

문서자료 및 다운로드

89600_Symbol_Table.exe 
89600 Symbol Table Example Program

FAQ 내용 2004-12-29

null EXE 258 KB