Here’s the page we think you wanted. See search results instead:

 

Parla con un Esperto

Can the 4395A/4396B read the cal data from the disk that comes with the cal kits such as the 85033D, 85039A, 85039B, etc?

No, the 4395A/4396B can't read the cal data from the disk furnished with these cal kits. But you can manually customize the definition of the Calibration Kit. For the details, please refer to the FAQ: What are the default calibration kit selections on the 4395A and 4396B Combination Analyzers?