Here’s the page we think you wanted. See search results instead:


Parla con un Esperto

Can I hide the softkey menu when I perform "Dump Screen Image" on the ENA / ENA-L?

(SUPPORTED MODELS IN BOLDE5071C  E5070B/71B  E5070A/71A  E5061A/62A E5061B E5072A)


  1. Press the hardkey of "Entry off (softkey on/off)" in order to hide the softkey.
  2. Press the hardkey of "system (capture)", so the image without the softkey displayed on the LCD screen is temporarily saved into the internal memory (clipboard).
  3. Press the softkey of "Dump Screen Image" (system > Dump Screen Image) "to save the screen snapshot in the HDD or FDD".