Keysight Technologies is now an independent company trading on the NYSE | Learn more

 

Contact an Expert

N4010A WLAN IEEE 802.11a/b/g/n Video Series

N4010A Videos

N4010A IEEE 802.11a/b/g & n WLAN Video Series

The following videos demonstrate the N4010A Wireless Connectivity Test Set for IEEE 802.11a/b/g and n WLAN testing. The videos are divided into 3 categories:

  • N4010A IEEE 802.11a/b/g Test in the WLAN Virtual Front Panel
  • N4010A/N4011A IEEE 802.11n Test in the WLAN Virtual Front Panel
  • N4010A Programming for Automated WLAN Manufacturing Test

The first 2 topics cover the N4010A WLAN Virtual Front Panel, a benchtop testing tool for WLAN test. The programming videos describe and demonstrate the use of the N4010A WLAN Driver (DLL) for integration into a programming environment.

The videos serve as useful training tools and demonstrators for the N4010A, N4011A, N4010A WLAN Virtual Front Panel and the N4010A WLAN Driver (DLL). Starting with legacy WLAN test (IEEE 802.11a/b/g), the videos follow a logical structure, introducing the basics of test before leading towards more complex measurements. The IEEE 802.11n videos introduce alternative hardware and RF setup with the N4011A MIMO/Multi-port Adaptor being used alongside the N4010A. Finally, the N4010A WLAN Driver (DLL) is used to automate manual tests for those wishing to understand the basics of automated manufacturing test for production.

N4010A 802.11a/b/g Test

VideoTitleDescriptionNarrationLaunch Video
1"Connecting to N4010A Hardware"This video describes the N4010A WLAN Virtual Front Panel and connecting to the N4010A hardware for the first time.   Narration PDF3m45s / 2.3MB
  play video
2"Transmitter Testing : Auto range and Format Independent Measurements"This video introduces WLAN transmitter testing beginning with basic format independent measurements. The Auto Range feature is also used to show how easy it is to configure the N4010A to the signal output from the device under test.  Narration PDF4m12s / 2.6MB
  play video
3"IEEE 802.11b Transmitter Testing : DSSS Measurements"This video demonstrates WLAN DSSS transmitter testing. This includes DSSS Standards Measurements and Demod Measurements.   Narration PDF7m / 4MB
  play video
4"IEEE 802.11a/g Transmitter Testing : OFDM Measurements"This video demonstrates WLAN OFDM transmitter testing. This includes OFDM Standards Measurements and OFDM Demod Measurements.  Narration PDF7m / 4MB
  play video
5"IEEE 802.11a/g Transmitter Testing : Power vs. Time & Spectral Mask"This video shows the Power versus Time and Spectral Mask tabs in the N4010A WLAN Virtual Front Panel using IEEE 802.11a/g signals.  Narration PDF3m 9s / 2MB
  play video
6"IEEE 802.11a/b/g Receiver Testing"This video demonstrates the AWG Control tab in the N4010A WLAN Virtual Front Panel for WLAN receiver testing.  Narration PDF6m 22s / 4.3MB
  play video

N4010A/N4011A 802.11n Test

VideoTitleDescriptionNarrationLaunch Video
1"Choosing the Correct RF Test Setup for 802.11n Test"This video provides an introduction to 802.11n manufacturing test and how to correctly setup the device under test with test equipment. The video describes a recommended setup using the Keysight N4010A/N4011A solution and also which configurations should be avoided in order to make high quality multiple channel measurements.  Narration PDF12m 21s / 7.8MB
  play video
2"N4010A/N4011A 802.11n Sequential Capture Technique"This video provides an introduction to IEEE 802.11n manufacturing test methodology used by the N4010A test set and the N4011A MIMO/Multi-port adaptor. The methodology is referred to as the sequential capture technique.  Narration PDF6m 33s / 4.3MB
  play video
3"Connecting to the N4010A/N4011A Hardware"This video describes the WLAN Virtual Front Panel and connecting to the N4010A and N4011A for first time for IEEE 802.11n test.  Narration PDF4m 13s / 2.3MB

  play video
4"IEEE 802.11n Transmitter Testing : Auto range and Format Independent Measurements"This video introduces WLAN 802.11n transmitter testing beginning with basic format independent measurements. The Auto Range feature is also used to show how to configure the N4010A to the signal output from the device under test without any prior knowledge.   Narration PDF8m / 4.7MB
  play video
5"IEEE 802.11n Transmitter Testing : 11n Demod"This video demonstrates IEEE 802.11n demodulated results for a 2x2 device. Individual channel characteristics are presented.  Narration PDF9m 17s / 19.7MB
  play video
6"IEEE 802.11n Transmitter Testing : Spectral Mask"This video shows an IEEE 802.11n Spectral Mask measurement in the N4010A WLAN Virtual Front Panel.  Narration PDF2m 5s / 4.4MB
  play video
7"802.11n Receiver Testing"This video shows you how to do IEEE 802.11n receiver testing in the N4010A WLAN Virtual Front Panel.  Narration PDF4m 37s / 9.9MB

  play video
8"Direct Map Mode and Spatial Expansion"Questions are commonly asked about the use of Direct Map Mode and Spatial Expansion when it comes to RF test, and compatibility with test equipment. These questions concern what is the best way to test, the impact on individual measurements and measurement integrity. This video discusses these subjects and shows results from a real device using Spatial Expansion and one using Direct Map mode.  Narration PDF13m / 10MB
  play video

N4010A Programming for Automated Manufacturing Test

VideoTitleDescriptionNarrationLaunch Video
1"N4010A WLAN Programming Overview"This video shows how the N4010A WLAN driver (DLL) can be used for producing your own automated test programs.  Narration PDF5m 41 s /11.3MB
  play video
2"N4010A WLAN Programming in 6 Basic Steps"This video describes how to use the WLAN driver for producing your own automated test programs. A C# programming example demonstrates the N4010A driver using a .NET interface.  Narration PDF17m 5s / 35.4MB
  play video