Here’s the page we think you wanted. See search results instead:

 

Discutez avec un expert

How do I start using the software provided with the 34405A Digital Multimeter for datalogging?

Follow the steps below to begin datalogging using the software provided with the 34405A Digital Multimeter:
1. Install the Agilent IO Libraries Suite from the CD that is shipped together with the instrument.
2. Connect the instrument to your PC or laptop
i. Connect the instrument to the USB port(s) on your PC or laptop with a USB 2.0-compliant USB cable, even if you are using USB 1.1 operations.
ii. Click Start> All Programs> Agilent IO Libraries Suite>Agilent Connection Expert to launch the Agilent Connection Expert.
iii. Turn on the instrument you connected. The Agilent Connection Expert will automatically detect the instrument. The "Assign USB device alias" window will pop-up, as shown below.

 

34405A

iv. Assign a different Alias Name if you want to. Then, click OK.
v. Double-click the Agilent IO Control icon at your PC/laptop's task bar, as shown below.

 

34405A

The "Agilent Connection Expert" window will appear, as shown. It will show that the instrument is connected to your PC or laptop.

34405A

3. Install the Intuilink software from the Product Reference CD that is shipped together with the instrument.
4. Establish a connection between the instrument and the Intuilink software.
i. Open Microsoft® Excel and activate the Intuilink toolbar from View -> Toolbars -> Agilent Intuilink Multimeter

34405A

ii. Click on the Connect button in the Intuilink toolbar, as shown below, to initiate a connection.

34405A

The "Connect to Multimeter" window will appear, as shown below.

34405A

iii. Select the USB address and click on the Identify Instrument(s) button. You will see the 34405A multimeter on your computer.
iv. Click on the Connect button. The status will show as "Connected" when connection has been established.
v. Close the dialog box once connected.
5. Setup the Intuilink to datalog a specific measurement
i. Ensure that the test lead or E2308A thermistor probe is connected to the input terminal of the instrument.
ii. Click on the Set Up Multimeter button on the Intuilink toolbar. The "Set up Multimeter" window will appear, as shown below.

34405A

iii. In the "Set up Multimeter" window, select a function, measurement range and resolution. Then, click OK.
iv. Click on the Set up/Run Logging Worksheet button on the Intuilink toolbar. The "Set up/Run Logging Worksheet" window will appear, as shown below.

34405A

v. In the "Set up/Run Logging Worksheet" window, enter the logging interval and duration for the intended datalog. Then, click OK.
Datalogging will start automatically, as shown in the example below.

34405A

Related Links