Here’s the page we think you wanted. See search results instead:

 

Discutez avec un expert

When using my Keysight 4294A impedance analyzer via Keysight IntuiLink 4395A/4396B/4294A, my Microsoft Excel application reports the Error "Failed to Capture State from Instrument." Can you advise?

 

The error message as shown below is displayed when the version of the 4294A firmware is lower than Rev 1.11.

Captured Error

 

The following instruction on the supported instruments is described on the Keysight IntuiLink 4395A/4396B/4294A support homepage:

Supported Instruments