Here’s the page we think you wanted. See search results instead:

 

Discutez avec un expert

On ENA, when I perform both the calibration with frequency offset off and the scalar-mixer calibration with frequency offset on, which calibration is valid?

(SUPPORTED MODELS IN BOLD: E5071C E5070B/71B E5070A/71A E5061A/62A E5061B E5072A)

If the frequency offset function is turned on, the scalar-mixer calibration data is used.
When you turn off the frequency offset function, the ENA uses the calibration data with frequency offset off, but still keeps the scalar-mixer calibration data in its memory.