Here’s the page we think you wanted. See search results instead:


Discutez avec un expert

Why do I see error 772 when I power-on or reset my E1441A Arbitrary Waveform Generator?

There was a production problem with the E1441A cards in 1998 where no valid setup was stored in non-volatile memory location 0. This caused the error 772 (non-volatile memory error) to occur. The easy fix for this problem is to send the following three commands to the instrument:



*SAV 0

These commands will cause a valid entry to be stored in memory location 0, and the problem will be permanently fixed.

This problem was corrected in production in June, 1998.