Here’s the page we think you wanted. See search results instead:

 

Hable con un experto

What is the bandwidth of the I.F. output on the mmW EXA?

The mmW EXA's offer option CR3 as the 2nd I.F. Output.  At frequencies ≤3.6 GHz the bandwidth is up to 140 MHz (nominal).  Above 3.6 GHz the bandwidth will be limited by the preselector bandwidth because option MPB (Microwave Preslector Bypass) is not currently available on the mmW EXA.  Therefore, the bandwidth above 3.6 GHz will be ~50 MHz.

Refer to the "Preselector Bandwidth" sectio in the EXA Specification Guide for more details.