Here’s the page we think you wanted. See search results instead:

 

Sprechen Sie mit einem Experten

Sample Programs for the E5061A/E5062A

Overview 

This is a sample program which is described in the Programming Manual. This is the same one stored in the furnished CD-ROM.

Revision Number 

See the revision number in each program.

Documents & Downloads

Sample Programs for the E5061A/E5062A - GPIB/LAN Programming 

Programming Example 2008-06-25

null ZIP 231 KB
Sample Programs for the E5061A/E5062A - VBA Programming 

Programming Example 2008-06-25

null ZIP 61 KB
The VBA Utility Program for option 100 

Programming Example 2012-11-15