Here’s the page we think you wanted. See search results instead:

 

Sprechen Sie mit einem Experten

What accessories should I order with the 8166XA DFB Laser?

An 816x mainframe is required to operate a DFB Laser Source Module. Additionally, a connector adapter in the 81000xI series is required for each 8166xA-series DFB laser source. These allow connection to many of the industry standard connectors.
NOTE: The output ferrule of these sources is angled, and is therefore compatible only with angled connectors, e.g., FC/APC, SC/APC, etc., and will therefore determine which of the interfaces can be used.

Related Information connector adapter in the 81000xI series