Here’s the page we think you wanted. See search results instead:

 

Sprechen Sie mit einem Experten

What is the difference between the 44727A, 44727B, and the 44727C?

The only differences between the three cards are jumper and switch settings on the module and the terminal block. The hardware is exactly the same otherwise. They were set up this way so that customers may order them already configured to current, voltage, or both without worrying about configuring the jumpers.