这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

Does Keysight i3070 automatically generate a boundary scan test for Self monitoring cell?

Yes, If there were a Self monitoring cell on a device pin that did not connect to another Boundary Scan device pin, there will still be silicon node declared in the generated interconnect test. In this case, the Boundary-Scan driver and receiver happen to be the same device and pin.


In the 'fault-dictionary' type information at the end of the 3070 interconnect VCL or in the ".x" file, there is terminology such as 'Monitor PO', where this self-monitoring structure exists.