Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

How do I transfer trace data to a PC from a Keysight CSA using VEE?

The examples below demonstrate the use of the remote commands for transferring trace data from the instrument. These can be downloaded and run using VEE 7.0 or later. If you are not using VEE and you would like to see what instrument remote commands are required to do this you can view the image files instead for a look at what the program contains.

There are two example that can be downloaded. One is a simple example that only transfers the trace data itself. The other also uses instrument parameters to configure the data display according to its current settings.

If you do not currently have a copy of Keysight VEE, you can go to the VEE web site to find out more about it as well as download a free 30 day trial version:

Documents et téléchargements

N1996A CSA Simple VEE Trace Date Example 
Simple example taking trace data only...

Programming Example 2006-04-25

For those not using VEE...

FAQ Content

66 Bytes
N1996A CSA VEE Trace Date Example 
Example using instrument parameters...

Programming Example 2006-04-25

For those not using VEE...

FAQ Content

133 Bytes
N1996A CSA Spectrum Analyzer User's and Programmer's Reference 
User's and programmer's reference information for the N1996A CSA spectrum analyzer.

Manuel de l'utilisateur 2007-03-01

null PDF 7.16 MB