Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

Keysight T&M Toolkit by Microsoft Visual Studio Version

Each Keysight T&M Toolkit version is supported for use with the Microsoft® Visual Studio® development environment versions shown on the following matrix. You can write your T&M Toolkit code in Visual Basic, C#, or Managed C++ except as noted in the matrix. T&M Toolkit can be used with the Standard and Pro Editions of the Visual Studio configurations provided by Microsoft, e.g. Standard Editions, Pro Editions, etc. You must be sure to use the correct version of Visual Studio according to the table below.

Operating System
T&M Toolkit Version Visual Studio 2002Visual Studio 2003Visual Studio 2005
1.0Yes (no Managed C++)NoNo
1.1Yes (no Managed C++)Yes (no Managed C++)No
1.2YesYesNo
2.0NoYesNo
2.1NoNoYes

Yes = Supported
No = Not Supported

Microsoft is a U.S. registered trademark of Microsoft Corporation.
Visual Studio is a registered trademark of Microsoft Corporation in the U.S. and/or other countries.