Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

Can I use the 16092A with the 4395A/4396B/4287A/E4991A?

Yes, you can use the 16092A with the 4395A/4396B/4287A/E4991A.
In order to use the 16092A with these instruments, it is necessary to set the Electrical Length to 3.4 mm by using the "user fixture" menu of the respective instrument.
For the details about how to define "user fixture", please refer to the following instrument manuals.

4395A Operation Manual (Page 7-17)

4396B Option 010 Operating Handbook (Page 3-2)

4287A Operation Manual (Page 149)