Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

What are the measurement intervals for the W-CDMA, cdma2000, and 1xEV-DO QPSK EVM measurements for E4406A and the PSA Series? Is the 12.2k Reverse Measurement Channel supported for W-CDMA?

In the A.04.07 release of the PSA Series firmware and the A.06.03 release of the E4406A, the measurement intervals for the QPSK EVM measurement as follows:

  • cdma2000 (Option B78) - 128 to 1536 chips
  • W-CDMA (Option BAF) - 128 to 2560 chips (1 slot)
  • 1xEV-DO (Option 204) - 32 to 2048 chips

The W-CDMA personality does support uplink 12.2 k RMC (Reverse Measurement Channel) in the QPSK EVM measurement.

Documents et téléchargements

E4406A VSA Transmitter Tester Firmware 
Free firmware update for E4406A VSA Series Transmitter Tester.
Versions antérieures

Computer Software Version courante: A.10.08 | 2007-08-13

PSA Series Spectrum Analyzer Firmware 
Firmware files for the E4440A, E4443A, E4445A, E4446A, E4447A, E4448A PSA spectrum analyzers.
Versions antérieures

Instrument Firmware/Software Version courante: A.11.21 | 2012-07-22