Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

ADS 2008 Update 1 Software Patches/Hotfixes

Keysight EEsof EDA will from time to time release hotfixes to address specific issues in a release. These hotfixes must be installed on top of an existing installation of ADS 2008 Update 1.

Please read the installation instructions supplied with the hotfix download to install the hotfix.

ADS 2008 Update 1 License Hotfix

 

Overview
If you have received new or renewal licenses that include any of the new ADS bundled licenses and/or elements, you will be instructed to download and install a licensing hot fix.

This hot fix is required to:

1. Enable your new licenses to work seamlessly with the ADS 2008 Update 1.

2. Address a timeout issue with Design Guides.

NOTE: An updated version of this licensing hot fix is available as of April 2009 to address the timeout issue with Design Guides. For customers that have already installed the initial version of the licensing hot fix prior to April 2009, please install the updated version.

For additional information, please visit: How do I use the new ADS Bundled Licenses and Elements?

3. The following downloads require ADS 2008 Update 1 version to be installed: