Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

What applications and measurements today require the mmW EXA's?

There are customers that require frequency coverage beyond 26.5 GHz but below 32/44 GHz. 

Applications include:

  • Radar/EW, LMDS (Local Multiport Distribution System) networks
  • Satellite communications
  • Wireless backhaul

Measurements include:

  • 2nd harmonics of signals in the Ku-Band (12-18 GHz)
  • 2nd harmonics at the lower end of the K-Band (15-26.5 GHz)
  • 3rd harmonics of X-Band (~7-12 GHz)

Applications that require the frequency coverage beyond 44 GHz can use a combination of external mixer with the mmW EXA that has option EXM, External Mixing.