Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Sample program files: E5061B ENA Custom Multiport Switch Solution using L4491A (5990-9359EN)

Overview:

This is the sample VBA program and the switch configuration file which is referred in the application note "Design Tutorial: E5061B ENA Custom Multiport Switch Solution using L4491A" (5990-9359EN).

How to install and run this file:

Copy the download .vba and .csv file to the D:\VBA folder of your E5061B. To run the macro, press [Macro Setup] on the E5061B front panel, then select Load & Run, and click on "MultiportControl_E5061B_xxxx" on the softkey menu.
 

Documents & Downloads

MultiportControl_E5061B_0100.vba 

Programming Example 2011-10-24

null EXE 82 KB
SW_Config_E5061B.csv 

Programming Example 2011-10-24

null XLS 2 KB
Design Tutorial: E5061B ENA Custom Multiport Switch Solution Using L4491A 
This application note describes how to configure a 12-port custom switch box with the L4491A switch platform and operation basics using the E5061B network analyzer.

Application Note 2011-11-29

null PDF 1016 KB