这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

航空航天与国防

此内容需要使用支持JavaScript的浏览器和Adobe Flash Player

获得Flash 

集中精力完成重要任务

航空航天与国防行业的任务正在不断发展和变化,但是有一点始终未变,那就是必须要保证那些从事危险工作的人员的人身安全。这项任务能否成功,取决于人员和技术如何适应变化,实现完美融合。随着系统技术日趋复杂,达到这一目标也变得越来越困难。

是德是您成功完成任务的保证。借助是德在测量科学和测试流程中的专业技术,您可以腾出更多时间来处理更重要的问题:执行当前任务并按计划转向未来任务。有是德保证您的系统就绪,您完全可以高枕无忧,从而集中精力完成更重要的任务。

有关是德在航空航天/国防领域的作用的更多信息,请下载免费手册 《是德在航空航天与国防领域的作用》。

查看测量解决方案实例有源天线测试多发射机环境测试信号

缩小范围

去除所有优化

行业/技术

按内容类型

按产品类别

1-10 / 10

排序:
Solving Mobile Radar Measurement Challenges 
This Microwave Journal article examines an alternative simulation method that allows for better cross-domain modeling in a single framework, to capture the complete effects of modern radar system performance.

文章 2016-06-13

 
Phased array beamforming software design, test, and measurement kit introduced by Keysight 
Military & Aerospace Electronics article introduces the W1720EP phased array radar beamforming kit add-on software simulation personality for the SystemVue 2016.08 design and test and measurement environment.

文章 2016-06-13

 
Digital Predistortion Linearizes Wireless Power Amplifiers 
This Article by Wan-Jong Kim, Shawn P. Stapleton, Jong Heon Kim, and Cory Edelman focuses on how digital predistortion linearizes wireless power amplifiers.

文章 2014-07-31

PDF PDF 1.81 MB
Addressing the Challenges of Radar and EW System Design and Test using a Model-Based Platform 
Article reprint, High Frequency Electronics, October 2013. Due to the challenges of Electronic Warfare (EW) environments, today’s designers require a solution for designing, verifying and testing their Radar and EW systems in an effective way.

文章 2013-10-10

PDF PDF 1.45 MB
Enabling Simulation and Test of Custom OFDM Signals 
Orthogonal frequency division multiplexing (OFDM) has become attractive for many current and emerging commercial applications because it provides a combination of data throughput, scalability, and robustness.

文章 2013-04-01

 
Testing Radar and EW Systems for the Real-World 
The solutions described in this Microwave Journal article do more than address a wide range of present and future radar systems: They also help overcome organizational hurdles.

文章 2012-07-12

 
The Coming of Age of the Software Communications Architecture 
Microwave Jounral article reprint on Software Defined Radio (SDR) technology, development tools for complex waveforms and radio applications in aerospace/defense and commercial applications.

文章 2011-04-24

PDF PDF 1.61 MB
Addressing the Design and Verification Challenges of LTE 
Wireless Design magazine article on testing LTE.

文章 2009-02-25

PDF PDF 4.59 MB
Creating High-Performance SDR Architectures 
How to co-design RF architectures together with baseband signal processing to create high performance and flexible SDR architectures that can achieve the critical performance specifications necessary in the operational environment.

文章 2008-11-25

PDF PDF 806 KB
用于雷达和电子战系统的先进设计系统连接解决方案 

文章 2008-04-14

PDF PDF 3.80 MB