検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

携帯電話

原因究明。 それがすぐに可能です。 特別な現象が得られたことがすぐにわかります。 キーサイト・テクノロジーの礎は、優れたハードウェア、ソフトウェア、人材の融合です。 測定技術分野のリーダーとして75年以上の実績があるキーサイトが作成した測定器とデザインソフトウェアにお任せください。

新しい携帯電話テクノロジーと既存の携帯電話テクノロジーの両方に渡る革新が続くことで、モバイルネットワーク/デバイスのデザイン/テストにさまざまな問題が生じます。 キーサイト・テクノロジーは、世界有数の電子計測器メーカーとして、シミュレーション、研究開発、デザイン検証、プリコンフォーマンス、コンフォーマンス、製造から、ネットワークの配備およびサービス保証までのライフサイクル全体に渡る携帯電話のテスト/デザインソリューションを豊富に取り揃え、最先端を走り続けています。

キーサイトは、デザインに何を取り入れれば最新の携帯電話規格に準拠できるのかを知っています。 キーサイトは、3GPPなどの有力な無線規格団体や最先端の5Gフォーラム/コンソーシアムのメンバーとして活動しているので、従来の1Gから最新の4Gテクノロジーまでの規格に準拠した最先端の携帯電話のテスト/デザインツールを提供できます。また、シミュレーションやテストに関する5Gの研究に対応するデザイン/テストソリューションを豊富に取り揃え、常に業界をリードしています。

測定器は将来も使用できるようにデザインされているので、テクノロジーの変化に応じて容易に進化して、最先端の課題に対応できます。 今日の研究開発から製造および将来の配備まで一貫した測定技術が提供されるので、お客様の投資を有効に活用できます。

キーサイトのデザイン/テストのエンジニア/専門家は、お客様のチームに対するアドバイス、支援、強化を世界中で行うことができます。 5G携帯電話MIMO無線LANテストに関するキーサイトの専門知識は、技術記事、アプリケーションノート、ウェブキャストで今すぐご覧いただけます。

YouTubeビデオを見る 

26-50 / 108

並べ替え
Agilent Technologies Unveils System Design Tools for Satellite Communications and Navigation 
Agilent announces two reference libraries for SystemVue, its premier platform for communications and aerospace/defense systems design.

プレス資料 2013-06-03

 
Agilent Technologies Unveils Beidou GNSS Signal Simulation at International Wireless Symposium 
Agilent Technologies announced that it has enhanced the capabilities of its Signal Studio for Global Navigation Satellite Systems (GNSS) software and added real-time multi-satellite simulation of China's Beidou system.

プレス資料 2013-04-15

 
Agilent PXT Wireless Communications Test Set Selected by Tri-L Solutions for LTE Over-the-Air Test 
Agilent Technologies Inc. (NYSE: A) today announced that Tri-L Solutions Inc. has selected Agilent's PXT wireless communications test set and integrated it with Tri-L Solutions SmarTest measurement software for testing LTE over the air.

プレス資料 2013-04-08

 
Agilent Technologies Introduces Industry's First LTE-Advanced 8x8 MIMO Signal-Generation and Analysi 
Agilent Technologies Introduces Industry's First LTE-Advanced 8x8 MIMO Signal-Generation and Analysis Solutions

プレス資料 2013-01-03

 
Agilent Technologies and CATR (TMC) to Collaborate on TD-LTE MIMO  
Agilent Technologies Inc. (NYSE: A) announced a memorandum of understanding has been signed with the China Academy of Telecommunication Research (Telecommunication Metrology Center), or CATR (TMC). The two organizations have agreed to work together on TD-LTE MIMO over-the-air (OTA) test research.

プレス資料 2012-09-13

 
Agilent Technologies Announces Wireless Communications Test Set with Innovative Multiport Adapter 
Agilent Technologies introduced the E6607B EXT wireless communications test set and companion E6617A multiport adapter. Optimized for non-signaling testing, the EXT/MPA combination increases test throughput and reduces the cost of test in the manufacturing of current- and next-generation smartphones and tablets that contain multiformat and multiband technologies.

プレス資料 2012-08-01

 
Agilent Technologies Accelerates Early Wireless Design Verification with New Release of SystemVue 
Agilent will demonstrate SystemVue 2012.06 along with a range of solutions for everything from circuit-level modeling through system verification for general RF, microwave, 4G communications, and aerospace/defense applications at DAC2012 (Booth 313), June 3-7, in San Francisco. SystemVue 2012.06 will also be demonstrated at IMS 2012/IEEE MTT-S (Booth 1015), June 19-21, in Montr al, Canada. A range of premier partner solutions will be available on Agilent Avenue and throughout the event area.

プレス資料 2012-06-05

 
Agilent Technologies Announces Voice-over-LTE Test System Developed with Brüel & Kjær 
Transporting voice over a packet-based LTE cellular infrastructure poses challenges that make voice-quality testing essential. The Agilent and Brüel & Kjær solution combines standards-based test methods with real-world base station emulation, RF test and functional test to ensure that VoLTE phones will meet user's expectations.

プレス資料 2012-05-10

 
Agilent Technologies Introduces 6-GHz Signal Generators with Industry-Best Performance 
Today's aerospace/defense environment requires enhanced radar performance to detect weak signals at long distances. To provide the pure and precise signals needed to test these designs, the MXG uses an innovative triple-loop synthesizer to deliver phase noise performance of -146 dBc/Hz at 1 GHz and 20 kHz offset. For developers of radar components such as mixers and analog-to-digital converters, the MXG also features industry-leading spurious performance of -96 dBc at 1 GHz.

プレス資料 2012-05-01

 
Agilent Technologies Enhances FieldFox RF Analyzers with Options for Measuring Time Domains and Chan 
Agilent will demonstrate its new FieldFox options, along with solutions that cover everything from circuit-level modeling through system verification for general RF, microwave, 4G communications, and aerospace/defense applications at IMS 2012/IEEE MTT-S (Booth 1015), June 19-21, in Montr�al, Canada. A range of premier partner solutions will also be available on Agilent Avenue and throughout the event area.

プレス資料 2012-05-01

 
Agilent Technologies Named Oscilloscope Company of the Year 
The award is based on Frost & Sullivan's recent analysis of the oscilloscope market. Frost & Sullivan ranked Agilent as the No. 2 company in 2009, but its rapid revenue growth since then has made it the leader in market penetration.

プレス資料 2012-04-25

 
Agilent Technologies Introduces Wireless Link for Remote Monitoring and Data Logging with Handheld 
Agilent Technologies Inc. announced the introduction of a wireless connectivity solution that links up to three Agilent handheld digital multimeters to smartphones, tablets and PCs.

プレス資料 2012-03-01

 
Agilent Technologies Announces Test Software for Equipment Based on Altair TDD/FDD LTE Chipset 

プレス資料 2012-02-28

 
Agilent Technologies Announces 42-Mbps DC-HSDPA IP Data Throughput Solution for the 8960 Wireless 
The Agilent E5515E delivers sustained, end-to-end IP data throughput at 42 Mbps, flexible and comprehensive RF measurements, and improved hardware capability for future requirements, making it easy and fast to stress wireless devices and verify their performance at full data rates.

プレス資料 2012-02-14

 
Agilent Technologies to Demonstrate Industry-First R&D and Manufacturing Test Solutions 
Agilent Technologies will demonstrate its industry-first communications test and measurement solutions for LTE-Advanced, LTE, HSPA+, dual-carrier HSDPA, MIMO, multi-standard radio and voice over LTE, along with 2G/3G solutions for R&D, manufacturing and deployment at the Mobile World Congress in Barcelona, Feb. 27- March 1.

プレス資料 2012-02-13

 
ETS-Lindgren Announces Support of Agilent PXT Wireless Test Set for LTE Over-the-Air Testing 
Agilent PXT performs OTA tests to industry standards and allows user equipment (UE) developers to characterize and optimize the behaviour of their designs. The EMQuest/PXT solution is offered with all ETS-Lindgren AMS for the testing of wireless devices

プレス資料 2012-02-03

 
Agilent Technologies Announces Bluetest Support of Agilent PXT for LTE Over-the-Air Testin 
Agilent Technologies Inc. (NYSE: A) today announced that Bluetest AB now supports Agilent's PXT wireless communications test set. The Bluetest RTS (Reverberation Test System) uses the Agilent PXT test set to evaluate LTE devices over the air.

プレス資料 2012-02-02

 
Agilent Technologies Announces Industry's First Eight-Channel RF Measurement Solution Addressing LTE 
Agilent Technologies Inc. (NYSE: A) today introduced industry-leading enhancements to its N7109A multi-channel signal analyzer for emerging multichannel LTE, LTE-Advanced and MIMO RF measurement requirements, including LTE antenna beamforming and LTE-Advanced carrier aggregation.

プレス資料 2012-02-02

 
Agilent Technologies Introduces Innovative Multi-Measurement Signal Analyzer Capability for Wireless 
Agilent Technologies Inc. (NYSE:A) today announced that an innovative, new multi-measurement capability is being added to its 89600 VSA software, enabling simultaneous signal analysis of multiple carriers and signal formats for more efficient testing and deeper signal insight in wireless test.

プレス資料 2011-11-15

 
Agilent Technologies Introduces Industry's First 3GPP Release 9 Compliant MSR Signal 
Ideal for engineers manufacturing base stations and base-station components, the MSR measurement application enables one-button, standards-based testing per the RF requirements defined in the TR 37 series of the 3GPP Release 9 standard. It is the first and only 3GPP-compliant one-button measurement application on the market today to quickly and easily manufacture MSR base stations and base-station components.

プレス資料 2011-10-19

 
Agilent Technologies Introduces Wideband DPD Modeling Platform for LTE-Advanced, 802.11ac  
Agilent Technologies Inc. (NYSE: A) today announced the newest release of its W1716 Digital Pre-Distortion Builder (DPD) software, designed to enable the high levels of wireless performance necessary for emerging wideband standards such as LTE-Advanced and IEEE 802.11ac.

プレス資料 2011-08-31

 
Frost & Sullivan recognizes Agilent 
with the 2011 Award for Market Share Leadership for emerging as the leader in the global wireless test equipment market through a range of products, market-focused approach and customer-oriented solutions.

プレス資料 2011-05-26

 
Agilent Technologies Acknowledged for Leadership in Wireless Test Market  
Agilent Technologies Inc. (NYSE: A) has received this year's Frost & Sullivan award for market-share leadership in global wireless test equipment.

プレス資料 2011-05-25

 
Agilent Technologies Introduces Three New LTE Design Verification and Conformance Systems 
Agilent Technologies Inc. (NYSE: A) today announced its new design verification and conformance systems for LTE. The three systems extend Agilent's GS-8800 series for cellular design verification and conformance and are intended for engineers testing LTE devices to meet the TS 36.521-1 standard. All three use the Agilent E6621A PXT wireless communications test set as their core signalling engine.

プレス資料 2011-02-14

 
Agilent Technologies Announces LTE Wireless Communications Test Set for Manufacturing 
Agilent Technologies Inc. (NYSE: A) today announced the Agilent EXT wireless communications test set for wireless device manufacturing. The new Agilent EXT includes X-Series Measurement Applications and Sequence Studio software along with enhanced Signal Studio software to support the required testing of existing and emerging communication technologies such as LTE.

プレス資料 2011-02-14

 

前へ 1 2 3 4 5 次へ