这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

蜂窝测试

是德科技公司是全球领先的测试与测量公司,可以提供全方位的设计、测试和管理解决方案。这些解决方案覆盖整个蜂窝技术领域――从传统1G系统到3G系统(例如HSPA),再到3GPP 长期演进技术(LTE)和1xEV-DO。是德的产品适用于从早期设计与开发、批量制造到网络部署和服务保障的全过程。推动蜂窝技术的创新与发展,是德为您披荆斩棘!

查看相关视频(优酷) 

1-18 / 18

排序:
E6640A EXM Wireless Test Set Ready for Volume Production of LTE-A, 802.11ac WLAN Devices 
Agilent Technologies today announced the E6640A EXM wireless test set, which offers breakthrough manufacturing-test scalability in technology coverage, performance and capacity to test up to 32 cellular and wireless-connectivity devices in parallel.

新闻资料 2014-02-13

 
Agilent Technologies Announces Wireless Communications Test Set with Innovative Multiport Adapter 
Agilent Technologies introduced the E6607B EXT wireless communications test set and companion E6617A multiport adapter. Optimized for non-signaling testing, the EXT/MPA combination increases test throughput and reduces the cost of test in the manufacturing of current- and next-generation smartphones and tablets that contain multiformat and multiband technologies.

新闻资料 2012-08-01

 
Agilent Technologies Accelerates Early Wireless Design Verification with New Release of SystemVue 
Agilent will demonstrate SystemVue 2012.06 along with a range of solutions for everything from circuit-level modeling through system verification for general RF, microwave, 4G communications, and aerospace/defense applications at DAC2012 (Booth 313), June 3-7, in San Francisco. SystemVue 2012.06 will also be demonstrated at IMS 2012/IEEE MTT-S (Booth 1015), June 19-21, in Montr al, Canada. A range of premier partner solutions will be available on Agilent Avenue and throughout the event area.

新闻资料 2012-06-05

 
Agilent Technologies Enhances FieldFox RF Analyzers with Options for Measuring Time Domains and Chan 
Agilent will demonstrate its new FieldFox options, along with solutions that cover everything from circuit-level modeling through system verification for general RF, microwave, 4G communications, and aerospace/defense applications at IMS 2012/IEEE MTT-S (Booth 1015), June 19-21, in Montr�al, Canada. A range of premier partner solutions will also be available on Agilent Avenue and throughout the event area.

新闻资料 2012-05-01

 
Agilent Technologies Introduces 6-GHz Signal Generators with Industry-Best Performance 
Today's aerospace/defense environment requires enhanced radar performance to detect weak signals at long distances. To provide the pure and precise signals needed to test these designs, the MXG uses an innovative triple-loop synthesizer to deliver phase noise performance of -146 dBc/Hz at 1 GHz and 20 kHz offset. For developers of radar components such as mixers and analog-to-digital converters, the MXG also features industry-leading spurious performance of -96 dBc at 1 GHz.

新闻资料 2012-05-01

 
Agilent Extends PXA with Embedded LTE and HSPA+ Measurement Applications 

新闻资料 2010-02-15

 
Agilent Technologies Announces HSPA+, E-EDGE Test Capability for R&D Designers Testing 3GPP Mobile D 

新闻资料 2008-10-21

 
安捷伦最新软件选件可提供完整的驱动测试功能 

新闻资料 2008-08-25

PDF PDF 124 Bytes
安捷伦推出用于 3G 手机的射频完整一致性测试系统 

新闻资料 2008-08-22

 
Agilent Technologies Announces 5.7 Mbps HSUPA Data Analysis for Testing Category 6 

新闻资料 2008-07-21

 
安捷伦推出用于 6 类测试的 5.7 Mbps HSUPA 数据分析 

新闻资料 2008-07-21

 
安捷伦推出业界首款针对 3GPP 标准元器件的 HSPA+ 测试解决方案 

新闻资料 2008-04-22

 
Agilent Technologies Offers Industry-First HSPA+ Test Solution for 3GPP-Compliant Components  

新闻资料 2008-04-22

 
Agilent Technologies Automates UMTS Cellular Mobile Stress Test with New Interactive Functional Test 

新闻资料 2008-01-15

 
安捷伦利用最新交互式功能测试软件实现自动的 UMTS 蜂窝移动极限测试 

新闻资料 2008-01-15

 
Agilent Technologies to Demonstrate Comprehensive Communications Test Solutions at CTIA Wireless 200 

新闻资料 2007-03-12

 
安捷伦推出业界首款用于 UMTS 版本6、HSUPA 和 IP 架构 UMTS 的网络分析工具 

新闻资料 2007-02-12

 
Agilent Technologies Adds 7.2/2 Mbps HSPA IP Data Connection, HSUPA Measurement Capabilities that Su 

新闻资料 2006-07-27