这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

是德科技无线连接技术

WiMAX • 物联网 IoT • MIMO • 蓝牙 • 802.11 WLAN • NFC / EMV 测试 • 基于 WiMedia 的 MB-OFDM 超宽带 UWB 测试 • ZigBee • 数字视频

全新视野,可以瞬间拥有。而您立即知道,自己从此与众不同。是德科技依托独有的硬件、软件和人员组合,帮助您开启全新的测量视野。我们的测试设备和设计软件传承 75 年以上测量技术领先优势,是您可以信赖的可靠助手。新兴和现有的无线技术一直在持续不断地发展创新,这給设计人员设计和测试各种构建互联世界的元器件、模块和设备带来了新挑战。作为全球领先的电子测试测量公司,是德科技将继续站在这一领域的最前沿,提供跨越整个技术生命周期 ― 从仿真、研发、设计验证、预兼容性测试、一致性测试、制造到网络部署及服务保证 ― 的全系列测试和设计解决方案。

我们知道如何确保您的设计符合最新标准。作为负责定义技术标准的无线标准组织中最积极的成员,我们一直最先提供符合标准的无线测试和设计工具,范围覆盖从蓝牙到 60 GHz 802.11ad 的所有技术。我们坚持面向未来的仪器设计理念,使您可以更容易地适应不断变化的技术,始终屹立在技术的最前沿。利用从当前的研究和开发阶段到未来的制造和部署阶段一脉相承的测量技术,您的投资可以发挥最大的价值。我们的设计与测试工程师和专家可以为您提供切实可行、卓有成效的建议和协助,极大增强您在全球各地的团队的技术实力。我们还经常发布有关物联网5G蜂窝通信MIMOWLAN 测试等方面的白皮书、应用指南和网上直播,即时为您提供最新的专业技术。

查看相关视频(优酷) 

1-12 / 12

排序:
Dual Channel MIMO Measurements for WiMAX™ Wave 2 
In WiMAX Wave 2 systems, a variety of dual-channel measurements can provide essential insight into their operation and performance. Article written by Ben Zarlingo and linked with permission from Wireless Design and Development.

文章 2009-06-26

 
New Solutions Put Wireless To The Test 
Recent advances have made it possible for test vendors to provide off-the-shelf chipset-specific solutions for Wi-Fi, Bluetooth, and WiMAX RF test. Linked with permission from Mobile Dev & design.

文章 2009-06-11

 
MIMO and the Battle Between LTE and WiMAX™ 
Link to April 10, 2009 Microwave Journal executive interview with Andy Botka and Carla Feldman regarding the PXB MIMO Receiver Test and the broader issue of LTE and WiMAX development.

文章 2009-04-10

 
Test solutions soup up for 4G 
Link to April 9, 2009 Microwave Journal editorial. Test equipment manufacturers are providing more capability by relying on the latest hardware and software for feature-rich and easy to use solutions with impressive raw performance.

文章 2009-04-09

 
A Day in the Life of a Mobile WiMAX™ Handset 
April 2009 featured article in Microwave Products Digest

文章 2009-04-01

 
Using Base Station and MIMO Channel Emulators for Mobile WiMAX Devices 
This article describes how a channel emulator can be used to characterize the performance of a MIMO receiver. The testing was done in stages of increasing complexity, namely testing under AWGN conditions, MIMO testing with known static channels, and finally testing with channels chosen to represent “real world” behavior.

文章 2009-01-11

PDF PDF 1.37 MB
What Every RF Engineer Should Know: OFDM & WiMax 
Feature story by Janine Love.

案例分析 2008-12-27

 
Unraveling Modulation Quality in Mobile WiMAX™ Uplink and Downlink with Multiple Zones and Bursts 
An article written for Microwave Journal addressing the difficulty in ensuring that the modulation quality of the WiMAX radio is sufficient for optimum RF performance and that it will perform according to industry standards.

文章 2007-11-01

PDF PDF 762 KB
First Pass Accuracy with Momentum GX for WiMAX Design 
Archived article at Microwave Product Digest discussing the challenges for designers in meeting cost and power consumption goals, using 3D-Planar electromagnetic (EM) simulation technology.

文章 2007-11-01

 
WiMAX™: Plotting A New Path To Global Broadband Mobility 
Archived article at Canadian Electronics identifying innovations in test and measurement to support the innovations in the industry.

文章 2007-09-01

 
Validating IEEE 802.16e Designs With The Mobile WiMAX MIMO Library 
The IEEE 802.16e standard, often referred to as mobile WiMAX, specifies air interfaces for broadband wireless access (BWA) systems.

文章 2007-05-08

PDF PDF 524 Bytes
WiMAX™: The Next Generation of Broadband Wireless Access 
Article reprint from Electronics in Canada. This article provides anoverview of the 802.16 standard, theWiMAX forum, and key applications.

文章 2004-09-01

PDF PDF 428 KB