Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

MIMO Test

A challenging antenna technology, MIMO (Multiple Input, Multiple Output) is improving spectral efficiency (bit/sec/Hz), signal quality and cell coverage. MIMO is being used in multiple technologies including LTE-Advanced, WLAN and now being heavily investigated for new 5G technologies. Being a complex technology and an evolving standard for multiple technologies, MIMO provides hidden roadblocks and requires its own suite of measurements. Keysight's solutions are ready to enable deeper insights, especially as the standard evolves. In design and test, Keysight's solutions support innovation across new and existing technologies and allows engineers to transform ideas into reality.

MIMO Test Insights

Keysight RF and Digital Learning Center - A commitment to learning with industry experts

Explore YouTube Videos 

1-22 of 22

Sort:
MIMO Over-The-Air Research, Development, and Testing 
International Journal of Antennas and Propagation, May 2012 article provides information on the many challenges of identifying the optimal channel models and test method(s), for MIMO

Article 2012-05-09

 
Two-Stage Over-the-Air (OTA) Test Method for LTE MIMO Device Performance Evaluation 
International Journal of Antennas and Propagation, February, 2012, article introduces a novel, flexible, and cost-effective method for measuring MIMO OTA using a two-stage approach.

Article 2012-03-28

 
Tackling MIMO Design and Test Challenges for 802.11ac WLAN 
This article from Microwave Journal shows how the system engineer can use system simulation to help understand the design performance and design requirements needed to achieve transmitter system-level metrics such as EVM.

Article 2012-03-11

 
Caution: MIMO Test Challenges Ahead 
Article published by Wireless Design & Development on MIMO testing challenges and methods to achieve higher data rates such as two0 and four-channel MIMO.

Article 2010-09-20

PDF PDF 70 KB
What every engineer needs to know about MIMO operation and measurement 
Utilizing MIMO to its fullest potential requires the engineer to have basic knowledge of its operation and measurement. This EP&T article by Agilent boils this knowledge down into 9 fundamental facts.

Article 2010-09-15

 
The MIMO Antenna: Unseen, Unloved, Untested! 
Microwave Journal (August 2010) article (.pdf) written by Agilent’s Moray Rumney. With the shift of MIMO from theory to real world this article focuses on performance testing in real world conditions.

Article 2010-08-20

PDF PDF 693 KB
Measuring MIMO In LTE Tx And Rx Tests 
Find the right combination of LTE test instruments and techniques to evaluate the performance of Long Term Evolution (LTE) components and systems under real-world conditions. A link to the MWJ article by Agilent.

Article 2010-08-18

 
A primer on MIMO in LTE 
An article in Electronic Products, written by Agilent’s Jan Whitacre, exploring the special employment of multiple-input, multiple-output radios to utilize spectrum in Long Term Evolution (LTE) systems.

Article 2010-02-01

 
Using a design-to-test capability for LTE MIMO  
Article written for RF DesignLine by Keysight experts explains how system-level simulation helps engineers gain valuable insight into design sensitivities of LTE MIMO systems.

Case Study 2009-07-10

 
Dual Channel MIMO Measurements for WiMAX™ Wave 2 
In WiMAX Wave 2 systems, a variety of dual-channel measurements can provide essential insight into their operation and performance. Article written by Ben Zarlingo and linked with permission from Wireless Design and Development.

Article 2009-06-26

 
Understanding the Impact of Channel Effects on MIMO System Performance  
Link to article published in the March 2009 issue of Microwave Product Digest discusses unique test and measurement challenges of implementing MIMO in a wireless system

Article 2009-04-28

 
MIMO and the Battle Between LTE and WiMAX™ 
Link to April 10, 2009 Microwave Journal executive interview with Andy Botka and Carla Feldman regarding the PXB MIMO Receiver Test and the broader issue of LTE and WiMAX development.

Article 2009-04-10

 
Test solutions soup up for 4G 
Link to April 9, 2009 Microwave Journal editorial. Test equipment manufacturers are providing more capability by relying on the latest hardware and software for feature-rich and easy to use solutions with impressive raw performance.

Article 2009-04-09

 
Using Base Station and MIMO Channel Emulators for Mobile WiMAX Devices 
This article describes how a channel emulator can be used to characterize the performance of a MIMO receiver. The testing was done in stages of increasing complexity, namely testing under AWGN conditions, MIMO testing with known static channels, and finally testing with channels chosen to represent “real world” behavior.

Article 2009-01-11

PDF PDF 1.37 MB
Expert Advice: The Importance of Average vs. Peak Performance in Cellular Wireless 
The average efficiency of the cell remains much lower than the peaks. November 2008 article by Moray Rumney linked with permission by Microwave Journal.

Article 2008-11-17

 
Analyze Antenna Approaches for LTE Wireless Systems 
Multiple-antenna techniques are a large part of improved performance in LTE wireless systems, but they must be properly understood in order to be properly tested.

Article 2008-08-13

 
3GPP LTE: Introducing Single-Carrier FDMA  
This article, published in issue 4 of the Agilent Measurement Journal, describes single-carrier FDMA for 3GPP LTE.

Article 2008-01-01

PDF PDF 491 KB
First Pass Accuracy with Momentum GX for WiMAX Design 
Archived article at Microwave Product Digest discussing the challenges for designers in meeting cost and power consumption goals, using 3D-Planar electromagnetic (EM) simulation technology.

Article 2007-11-01

 
WiMAX™: Plotting A New Path To Global Broadband Mobility 
Archived article at Canadian Electronics identifying innovations in test and measurement to support the innovations in the industry.

Article 2007-09-01

 
Validating IEEE 802.16e Designs With The Mobile WiMAX MIMO Library 
The IEEE 802.16e standard, often referred to as mobile WiMAX, specifies air interfaces for broadband wireless access (BWA) systems.

Article 2007-05-08

PDF PDF 524 Bytes
Addressing the new challenges of MIMO wireless LAN manufacturing test 
Article reprint from RF Design. New test equipment and techniques can keep the testing costs within the range of that for 802.11a/g systems.

Article 2006-10-01

PDF PDF 1.18 MB
WiMAX™: The Next Generation of Broadband Wireless Access 
Article reprint from Electronics in Canada. This article provides anoverview of the 802.16 standard, theWiMAX forum, and key applications.

Article 2004-09-01

PDF PDF 428 KB