这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

MIMO测试

是德MIMO测试

作为全球著名的测试与测量解决方案提供商,是德一直引领着MIMO (多路输入多路输出)等新兴市场的发展潮流。MIMO是一种实现起来颇具挑战性的天线技术,但它最终将会提高频谱效率(比特/秒/赫兹)、改善信号质量、扩大覆盖范围。作为一种正在演进的标准,它现在还面临着许多隐藏的障碍,需要一套全新的测量解决方案。我们的工程师作为测试与测量领域的专家,正在帮助您更轻松地进行新型测量,对系统进行分析和故障诊断。从研发到集成和制造的各个阶段,是德都拥有卓越的测试设备,能够对这些复杂信号进行深入分析,使您能够按照预定时间实现市场目标。所以,当您推动MIMO的创新与发展时,是德为您排忧解难。

现在,移动WiMAX和802.11n WLAN标准都在实施MIMO。这些实施的具体信息和测试设备可在相应的网页上找到;

观看 YouTube 视频 

1-25 / 110

排序:
M9391A PXIe Vector Signal Analyzer 1 MHz to 3 GHz or 6 GHz - Data Sheet 
This data sheet contains specifications and other technical information related to the M9391A PXIe Vector Signal Analyzer.

产品资料 2015-07-10

89601B/BN-BHF Custom OFDM Modulation Analysis, 89600 VSA Software - Technical Overview 
89600 VSA software Option BHF enables OFDM measurements for analyzing custom OFDM formats, including FDD, TDD, MIMO and multi-user systems.

技术总览 2015-04-16

是德科技 LTE/LTE-A 多通道参考解决方案 
是德科技 LTE/LTE-A 多通道参考解决方案

手册 2015-03-09

PDF PDF 3 MB
M9391A PXIe Vector Signal Analyzer - Product Fact Sheet 
This document provides an overview of the technical and other benefits related to the M9391A PXIe Vector Signal Analyzer

手册 2015-02-17

PDF PDF 731 KB
Speed Time to Market with Consistent Measurements from R&D Through Manufacturing - Application Note 
This white paper describes the benefits of having a choice of bench top or modular instruments that are supported by common software applications.

应用说明 2014-11-17

N5106A PXB Baseband Generator and Channel Emulator - Configuration Guide 
This configuration guide offers assistance in the ordering process for the PXB, including convenient bundles and custom configurations.

配置指南 2013-11-25

PDF PDF 1.15 MB
AXIe and PXI Modular Test Solution for Multiband SATCOM Monitoring - Application Note 
This application overview will show how to simplify multiple satellite band monitoring and analysis using the Keysight AXIe M9703A high-speed digitizer, N5183A LO, and 89601B VSA software.

应用说明 2013-11-07

PDF PDF 1.16 MB
89601B/BN-BHJ, -B7R, -B7Z WLAN, 89600 VSA Software - Technical Overview 
Gain greater insight into wireless LAN signals with the 89600 VSA software for 802.11a/b/g/n/ac modulation analysis.

技术总览 2013-06-21

PDF PDF 3.43 MB
Design and Test Solutions for Medical Devices - Brochure 
This brochure showcases Keysight in the emerging Wireless Medical Devices market and provides descriptions on its broad and powerful medical design and test solutions as well as details on the market

手册 2013-05-09

PDF PDF 8.82 MB
Agilent PXT Wireless Communications Test Set Selected by Tri-L Solutions for LTE Over-the-Air Test 
Agilent Technologies Inc. (NYSE: A) today announced that Tri-L Solutions Inc. has selected Agilent's PXT wireless communications test set and integrated it with Tri-L Solutions SmarTest measurement software for testing LTE over the air.

新闻资料 2013-04-08

 
Multichannel Measurements in MIMO 802.11ac Baseband IQ Simulation, Design & Test - Application Note 
This solution brief will show Keysight Technologies' complete, end-to-end solution for multichannel measurements of 802.11ac BBIQ simulation, design and test.

应用说明 2013-04-05

PDF PDF 748 KB
Agilent Technologies Introduces Industry's First LTE-Advanced 8x8 MIMO Signal-Generation and Analysi 
Agilent Technologies Introduces Industry's First LTE-Advanced 8x8 MIMO Signal-Generation and Analysis Solutions

新闻资料 2013-01-03

 
N7109A多通道信号分析系统 
在新一代无线技术开发过程中,MIMO测量设备成为每个研发工程师必备的一种工具。从802.11n到LTEAdvanced及其以后的标准,AgilentN7109A多通道信号分析仪都能够以令人心动的价格为2通道、4通道和8通道系统提供出色的MIMO射频性能。

产品资料 2012-11-01

Agilent Technologies and CATR (TMC) to Collaborate on TD-LTE MIMO  
Agilent Technologies Inc. (NYSE: A) announced a memorandum of understanding has been signed with the China Academy of Telecommunication Research (Telecommunication Metrology Center), or CATR (TMC). The two organizations have agreed to work together on TD-LTE MIMO over-the-air (OTA) test research.

新闻资料 2012-09-13

 
MIMO Over-The-Air Research, Development, and Testing 
International Journal of Antennas and Propagation, May 2012 article provides information on the many challenges of identifying the optimal channel models and test method(s), for MIMO

文章 2012-05-09

 
Agilent Technologies Introduces 6-GHz Signal Generators with Industry-Best Performance 
Today's aerospace/defense environment requires enhanced radar performance to detect weak signals at long distances. To provide the pure and precise signals needed to test these designs, the MXG uses an innovative triple-loop synthesizer to deliver phase noise performance of -146 dBc/Hz at 1 GHz and 20 kHz offset. For developers of radar components such as mixers and analog-to-digital converters, the MXG also features industry-leading spurious performance of -96 dBc at 1 GHz.

新闻资料 2012-05-01

 
Two-Stage Over-the-Air (OTA) Test Method for LTE MIMO Device Performance Evaluation 
International Journal of Antennas and Propagation, February, 2012, article introduces a novel, flexible, and cost-effective method for measuring MIMO OTA using a two-stage approach.

文章 2012-03-28

 
Tackling MIMO Design and Test Challenges for 802.11ac WLAN 
This article from Microwave Journal shows how the system engineer can use system simulation to help understand the design performance and design requirements needed to achieve transmitter system-level metrics such as EVM.

文章 2012-03-11

 
深入分析无线连通性 
This WiCON brochure focuses on test solutions for WiMAXT, RFID, NFC, WLAN, Bluetooth®, UWB, ZigBee technologies.

手册 2011-10-17

PDF PDF 1.95 MB
MIMO Tx/Rx Test Solutions - Selection Guide 
For RF engineers working with MIMO implementations in LTE. Determine the right set of Keysight products to help validate MIMO coding and the quality of MIMO signal transmission.

选型指南 2011-05-31

PDF PDF 598 KB
Introduction of LTE-Advanced Signal Generation and Analysis at Mobile World Congress March 2011 
Keysight’s European Marketing Manager, Renaud Duverne, introduces new capabilities capabilities such as carrier aggregation and answers questions about LTE-A early adoption, reducing the cost of test, transformative technologies and the challenges of growing video traffic.

基本演示 2011-03-14

 
Demonstration of analysis of un-impaired and impaired WiMAX(TM) MIMO signal  
This video contains an analysis of a 2x2 WiMAX MIMO signals using the N7100 Multi-channel Signal Analysis Platform and the 89600 Vector Analysis Software. Both an un-impaired signal and signal impaired by pedestrian fading are examined.

基本演示 2011-03-02

 
利用是德科技提供的丰富资源,助您深入了解 MIMO 技术 
索取印刷海报、下载应用说明

促销资料 2011-03-02

 
Option B7Z IEEE 802.11n MIMO Modulation Analysis 89600 Vector Signal 
This demonstration guide provides step by step instructions for making 802.11n MIMO measurements using the 89600 VSA software.

基本演示 2011-02-25

Demonstration of analysis of un-impaired and impaired LTE MIMO signal 
This video contains an analysis of a 2x2 LTE MIMO signals using the N7100 Multi-channel Signal Analysis Platform and the 89600 Vector Analysis Software. Both an unimpaired signal and signal impaired by static fading are examined.

基本演示 2011-02-22

 

1 2 3 4 5 下一页