Here’s the page we think you wanted. See search results instead:

 

Discutez avec un expert

Manufacturing & Production Test

As the world rapidly transforms with new technologies constantly emerging in the market, engineers in the consumer electronics, industrial and medical industries rush to design products which incorporate the latest trends. The rate of change is increasing, and the pace of product innovation is expanding.

However, a few things remain unchanged, such as the need to reduce your product and design costs to improve margins, and to reduce your time-to-market in order to meet consumers’ increasing expectation for superior and modern products which evolve with the times.

Keysight can help. With our market-leading hardware and software, and over 75 years of test and measurement experience, let us help you solve your most difficult test challenges to keep you ahead of the curve.

51-75 of 114

Sort:
The Importance of Test and Inspection When Implementing Lead-Free Manufacturing 
Many papers, articles, and studies have been written about process issues, reliability issues, repair issues, and the merits of different alloys. This paper addresses the impacts on test and inspection when going lead-free.

Application Note 2004-08-20

PDF PDF 260 KB
Using Lead-Free PCB Finishes at Manufacturing In-circuit Test Stage 
The purpose of this document is to share experiences and educate engineers regarding different PCB surface finishes and the specific changes required in the PCB build process to allow for ICT.

Application Note 2004-08-08

PDF PDF 102 KB
Solder Paste Inspection - Organize the Pieces 
Published in Global SMT & Packaging, November 2003

Application Note 2003-11-01

PDF PDF 818 KB
Realizing the Benefits of 3D Inline Solder Paste Inspection 
Published in SMT Magazine/Germany, August 2003

Application Note 2003-08-01

PDF PDF 67 KB
Test Coverage: What Does It Mean when a Board Test Passes? 
Originally presented at the 2002 International Test Conference -- Characterizing board test coverage as a percentage of devices or nodes having tests does not accurately portray coverage, especially in a limited access testing environment.

Application Note 2003-07-28

PDF PDF 266 KB
3D Inline Solder Paste Inspection - Benefit Realized 
100% solder paste inspection helps to reduce the contribution from the print process to solder joint defects.

Application Note 2003-06-01

PDF PDF 59 KB
Solder Paste Inspection for the SMT line: 3D In-line Systems Come of Age 
Published in Electronic Production & Test, May 2003.

Application Note 2003-05-01

PDF PDF 115 KB
Testing Transformers on Unpowered Systems 
This paper explains how to test basic analog parts, using unpowered systems.

Application Note 2003-03-21

PDF PDF 10 KB
PLR and 5DX Customized Defect Names Implementation 
You can use customized defect names on both the 5DX and on the PLR. This is particularly valuable when you want to display defect names in a local language.

Application Note 2003-03-01

 
Boundary Scan Helps EMS Companies Cut Test Costs and Increase Revenues 
Electronics Manufacturing Services (EMS) providers can utilize boundary-scan to reduce test cost expenses and also generate additional revenue opportunities.

Application Note 2003-03-01

PDF PDF 242 KB
Using Boundary Scan to Link Design and Manufacturing Test 
By leveraging boundary-scan tests generated in Design and re-using them at Manufacturing Test, manufacturers can produce long-term benefits in terms of lower costs, greater efficiencies and higher quality products.

Application Note 2003-03-01

PDF PDF 502 KB
What to Consider When Selecting the Optimal Test Strategy 
This paper addresses several issues for selecting the optimal inspection strategy, presenting data from many studies that Keysight has performed in the quest to find the optimal test / inspection strategy.

Application Note 2003-03-01

PDF PDF 175 KB
Ground Bounce Basics and Best Practices 
This article offers a description of the physical properties that result in ground bounce during board test.

Application Note 2003-01-28

PDF PDF 138 KB
New Features in Version 5.0 Software for 3070 
Typically, when Keysight's Manufacturing Test Division introduces a new software revision for its flagship 3070 In-Circuit Tester, it only communicates with customers about the major new features.

Application Note 2003-01-28

PDF PDF 84 KB
System Issues in Boundary-Scan Board Test 
While Boundary-Scan is a powerful test tool, test engineers are finding out that yesterday's DFT rules and test approaches may actually be detrimental to successfully testing systems on a board.

Application Note 2003-01-28

PDF PDF 37 KB
Design for Testability - Test for Designability 
This paper addresses testability considerations, both physical and logical, and focuses on both the new constraints and the new freedoms of modern manufacturing test in the ever-changing challenge.

Application Note 2003-01-28

PDF PDF 852 KB
A New Process for Measuring and Displaying Board Test Coverage 
Written by Kenneth P. Parker, Keysight Technologies. First presented at Apex 2003, Anaheim, California.

Application Note 2003-01-01

PDF PDF 116 KB
When to Use AOI, When to Use AXI, and When to Use Both 
by Stig Oresjo, senior test strategy consultant at Keysight Technologies.

Application Note 2002-12-01

PDF PDF 70 KB
Optimizing Power Product Usage to Speed Design Validation Testing (AN 1434) - Application Note 
This 15-page application note presents methods and techniques to decrease setup time and test time.

Application Note 2002-11-22

Preparing a .cc File for Export to Test Link 
This procedure describes the process of converting ECAD data into a form that can be used by Test Link.

Application Note 2002-10-16

PDF PDF 70 KB
UNIX vs. Windows Differences for 3070 Users 
This documentation serves as a PC transition guide to help existing 3070 customers migrate from the Unix platform to the PC platform.

Application Note 2002-09-19

 
Windows & Unix Feature Comparison 
The Windows & Unix 3070 Feature Comparison document provides a detailed listing of features translated to the Windows based 3070 from the Unix based 3070.

Application Note 2002-07-31

PDF PDF 71 KB
3070 In System Programming (ISP) Family 
On Board Programming, Bottom Line Benefits

Application Note 2002-07-25

PDF PDF 200 KB
Remote Network Connections Creation for the Operator Logon 
Operator logon on the Keysight 5DX Series II System is limited, in that it does not allow Operator to make network connections that are required for sending images and res files to the PLR workstation.

Application Note 2002-06-30

 
Maintaining Power with Dual Stage Fixtures 
Occasionally there is a need to do dual stage fixturing where power must be maintained during parts of both stages.

Application Note 2002-06-07

PDF PDF 48 KB

Previous 1 2 3 4 5 Next