这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

仪器操作系统和软件

浏览我们在此提供的丰富应用指南,获得关于仪器操作系统和软件的重要信息。您可以找到最新版本和以前版本的应用指南。

还可了解我们的驱动程序、固化软件和软件

26-50 / 65

排序:
Keysight 3070 Now Powered by Industrial PC Controllers 
The Keysight 3070 is now controlled by PCs similar to others used in your production and office environment lowering system administration and learning costs.

应用说明 2003-01-23

PDF PDF 207 KB
Connecting a UPS to a 3070 Controller 
This paper describes how to connect a UPS to the 3070 testhead controller. It uses the Advanced Power Conversion Smart-UPS with PowerChute Plus software.

应用说明 2003-01-07

PDF PDF 87 KB
Preparing a .cc File for Export to Test Link 
This procedure describes the process of converting ECAD data into a form that can be used by Test Link.

应用说明 2002-10-16

PDF PDF 70 KB
UNIX vs. Windows Differences for 3070 Users 
This documentation serves as a PC transition guide to help existing 3070 customers migrate from the Unix platform to the PC platform.

应用说明 2002-09-19

 
Windows & Unix Feature Comparison 
The Windows & Unix 3070 Feature Comparison document provides a detailed listing of features translated to the Windows based 3070 from the Unix based 3070.

应用说明 2002-07-31

PDF PDF 71 KB
3070 In System Programming (ISP) Family 
On Board Programming, Bottom Line Benefits

应用说明 2002-07-25

PDF PDF 200 KB
Remote Network Connections Creation for the Operator Logon 
Operator logon on the Keysight 5DX Series II System is limited, in that it does not allow Operator to make network connections that are required for sending images and res files to the PLR workstation.

应用说明 2002-06-30

 
Using NDFCOL.EXE, the NDF "Line Up the Columns" Utility 
NDFCOL.EXE is a handy little utility that will form neat columns of data in NDF files.

应用说明 2002-06-06

 
Obtaining a Listing of Applications on Series II Systems 
There is currently no easy way to obtain a list of all resident applications on a 5DX System or TDW. It is difficult to match panel name with hash name and see when the application was last updated.

应用说明 2002-06-01

 
Sampling on the Keysight 5DX 
Sampling Mode allows test coverage to be optimized with line speed. This document explore the setup procedure for the Keysight 5DX for sampling.

应用说明 2002-05-08

 
PLD Programming on the Keysight 3070 Using the PLD ISP Product 
In-System Programmable PLDs are more widely used on today's boards to provide flexibility to design engineers and to reduce the cost of a product.

应用说明 2002-02-26

PDF PDF 242 KB
The Life of a 5DX Inspection C# File 
The {Hashed Panel Name}.C# file is basically cad information about a panel program. It is used in conjunction with various utilities to overlay cad data on images or provide cad data for filters.

应用说明 2001-10-16

PDF PDF 97 KB
Synchronizing 3070 System Clocks 
These instructions are for synchronizing the system clocks of several network-connected UX workstations in the absence of an existing timeserver.

应用说明 2001-09-27

PDF PDF 66 KB
3070 Series 3 Flash70 Programming Guide 
This guide contains information about the procedures, tasks, and syntax required to perform flash programming with HP 3070 test systems.

应用说明 2001-09-12

PDF PDF 1.85 MB
Version 7.x ASAP Best Practices  
In an effort to standardize programming practices for the Keysight 5DX, Keysight has created a set of procedures representing 5DX "best practices" that address various aspects of the programming process.

应用说明 2001-07-25

 
In-System Programming on the Keysight 3070 
In-System Programmable devices are more widely used on today's boards to provide flexibility to design engineers and to reduce the cost of a product.

应用说明 2001-07-02

PDF PDF 205 KB
Tying a Power Supply to Multiple Boards in a Panel 
If you have a situation with multiple boards on a panel, and you need to wire one or more power supplies to each board, you often can wind up with problems wiring power and ground. Usually, you'll see warnings of the type FXT66.

应用说明 2001-06-12

PDF PDF 16 KB
Writing Flash Memory with Keysight 3070 Systems 
Flash memory is traditionally programmed on PROM programmers, but some manufacturers report a one percent damage rate due to the extra handling steps required!

应用说明 2001-05-18

PDF PDF 31 KB
Rotating Boards on a Panel 
Rotating Boards on a Panel if often necessary. In addition to the software revisions named within, the explained technique in the document is utilized for for 4.x, 5.x, 6.x and 7.x. For 8.x Test Link deals with this automatically.

应用说明 2001-05-17

PDF PDF 40 KB
Reducing Process Defect Escapes with Vectorless Test 
Process defects that escape in-circuit test lead at best to increased repair costs, and at worst to a "bone pile1" problem.

应用说明 2001-05-17

PDF PDF 512 KB
Dealing with Board Thickness Variations 
The Keysight 5DX has the capability to be implemented such that it can accommodate thickness variations on a board-by-board basis. NOTE: Content described is in the 5DX Reference Guide but is no longer in Chapter 7 as mentioned herein.

应用说明 2001-05-16

PDF PDF 31 KB
Use of Wrong Thickness Technique Gives Bad Test Results 
Beginning with release 6.0, there are two techniques for measurement of solder thickness on the Keysight 5DX, each based on use of a different Confirmation & Adjustment panel.

应用说明 2000-12-31

 
Hybrid32 Migration 
This document is provided to help users of HybridPlus Pin Cards more easily incorporate the Hybrid32 technology into their existing systems.

应用说明 2000-11-01

PDF PDF 61 KB
Learned Data for the 5DX 
The Keysight 5DX uses learned data in several ways to improve algorithm performance. There are basically 2 different forms of learned data.

应用说明 2000-11-01

 
Converting 8924C software for the E8285A 
This Product Note assumes you are converting software originally written for the Keysight 8924C, for use with the Keysight E8285A. Ideas are also included for modifying your software to function interchangeably with both the 8924C and the E8285A. This Note is meant to supplement the information...

应用说明 2000-07-01

以前 1 2 3 下一页