这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

部件和特殊设备

1-25 / 48

排序:
是德科技 Mini 在线测试仪 
是德科技 Mini 在线测试仪

应用说明 2016-04-06

Boundary Scan DFT Guidelines for Good Chain Integrity and Test Coverage - Application Note 
This application note provides some key guidelines to enable good design for testability using boundary scan.

应用说明 2016-01-21

PDF PDF 1.99 MB
使用 Medalist VTEP v2.0-VTEP、iVTEP 和 NPM 使测试范围最大化 
使用 Medalist VTEP v2.0-VTEP、iVTEP 和 NPM 使测试范围最大化

应用说明 2015-12-22

“Shotgunning”, a Bad Fit for Lead-Free Test 
Shotgunning, a common repair technique in functional test, will be negatively affected by lead-free processes. This article explores the technique and draws broad conclusions regarding the impact of lead-free on electronics manufacturing test

应用说明 2015-07-14

PDF PDF 99 KB
Detecting Tailgating Boards on the i3070 Inline In-Circuit Tester - Application Note 
Tailgating sensor improvements on the Keysight i3070 Series 5i inline in-circuit tester help to further minimize damages due to operator and upstream loading errors.

应用说明 2015-01-05

PDF PDF 437 KB
使用 i1000D SFP 在线测试系统 测试汽车保险丝盒 
使用 i1000D SFP 在线测试系统 测试汽车保险丝盒

应用说明 2014-08-06

Modifying DDR Libraries for Silicon Nail Test Generation on the Keysight x1149 Boundary Scan Analyzer 
This application note describes how to modify DDR libraries to generate silicon nails tests on the Keysight x1149 Boundary Scan Analyzer.

应用说明 2014-08-03

PDF PDF 1.57 MB
Releasing the “Test Sequence” and “Test” to Production on the Keysight x1149 Boundary Scan Analyzer 
This application note describes how to release test sequences and tests to production when using the Keysight x1149 Boundary Scan Analyzer.

应用说明 2014-08-03

PDF PDF 5.52 MB
Offline vs Inline: Shifting to automated inline ICT - White Paper  
This paper discusses the benefits of adopting an inline in-circuit test strategy for electronics manufacturers looking to increase product quality and reliability while ensuring optimal ROIC.

应用说明 2014-05-14

How to build a fixture for use with the Keysight Cover-Extend Technology 
Cover-Extend Technology is Keysight’s latest limited access solution for in-circuit test. This paper documents the necessary information for a fixture vendor to build a Cover-Extend fixture.

应用说明 2011-06-24

PDF PDF 1.09 MB
Network Parameter Measurement: Best Practices using the Keysight Medalist i3070 
This paper describes how to maximize benefits from the Network Parameter Measurement capability on the Keysight Medalist i3070 in-circuit test system using enhancements in software version 7.20p.

应用说明 2009-04-02

PDF PDF 55 KB
Medalist i3070 In Circuit Test – Utilizing the most comprehensive Limited Access 
This article introduces the seven most prominent and effective limited access tools on the Keysight Medalist i3070 ICT, collectively known Super 7 suite.

应用说明 2009-03-06

PDF PDF 342 KB
High Node Count Fixturing Solutions for Keysight Short-Wire Test Fixtures 
This paper discusses problems encountered in building large, high node count vacuum actuated test fixtures for the Keysight 3070 family of board test systems.

应用说明 2008-04-30

PDF PDF 67 KB
The Future of In-Circuit Testing in the High-speed, Complex Electronics Environment 
As board complexity and node counts continue to rise and high speed differential signaling continues to grow in popularity, In-Circuit Test needs to move quickly beyond the traditional realms. This article explores this in detail.

应用说明 2007-10-31

Making the Most of Keysight Throughput Multiplier on Medalist In-Circuit Test Systems 
Keysight Throughput Multiplier reduces test time on in-circuit test systems by testing up to four boards of a single-board-type panel simultaneously. The tips in this application note will help users make the most of this valuable tool.

应用说明 2007-10-12

 
In-circuit Testing of Low Voltage Devices 
Core technical document summarizing issues regarding the testing of low voltage devices on the 3070 and i5000, including updated Safeguard information.

应用说明 2005-05-25

PDF PDF 172 KB
Test and Inspection as Part of the Lead-free Manufacturing Process 
The paper addresses issues that will impact defect levels and defect spectrum during the transition to lead-free manufacturing. It also addresses different test and inspection systems’ readiness to test lead-free printed circuit board assemblies.

应用说明 2005-02-22

PDF PDF 421 KB
The Importance of Test and Inspection When Implementing Lead-Free Manufacturing 
Many papers, articles, and studies have been written about process issues, reliability issues, repair issues, and the merits of different alloys. This paper addresses the impacts on test and inspection when going lead-free.

应用说明 2004-08-20

PDF PDF 260 KB
Using Lead-Free PCB Finishes at Manufacturing In-circuit Test Stage 
The purpose of this document is to share experiences and educate engineers regarding different PCB surface finishes and the specific changes required in the PCB build process to allow for ICT.

应用说明 2004-08-08

PDF PDF 102 KB
Test Coverage: What Does It Mean when a Board Test Passes? 
Originally presented at the 2002 International Test Conference -- Characterizing board test coverage as a percentage of devices or nodes having tests does not accurately portray coverage, especially in a limited access testing environment.

应用说明 2003-07-28

PDF PDF 266 KB
Testing Transformers on Unpowered Systems 
This paper explains how to test basic analog parts, using unpowered systems.

应用说明 2003-03-21

PDF PDF 10 KB
Boundary Scan Helps EMS Companies Cut Test Costs and Increase Revenues 
Electronics Manufacturing Services (EMS) providers can utilize boundary-scan to reduce test cost expenses and also generate additional revenue opportunities.

应用说明 2003-03-01

PDF PDF 242 KB
What to Consider When Selecting the Optimal Test Strategy 
This paper addresses several issues for selecting the optimal inspection strategy, presenting data from many studies that Keysight has performed in the quest to find the optimal test / inspection strategy.

应用说明 2003-03-01

PDF PDF 175 KB
Using Boundary Scan to Link Design and Manufacturing Test 
By leveraging boundary-scan tests generated in Design and re-using them at Manufacturing Test, manufacturers can produce long-term benefits in terms of lower costs, greater efficiencies and higher quality products.

应用说明 2003-03-01

PDF PDF 502 KB
Ground Bounce Basics and Best Practices 
This article offers a description of the physical properties that result in ground bounce during board test.

应用说明 2003-01-28

PDF PDF 138 KB

1 2 下一页