Sprechen Sie mit einem Experten

Conformance WiMAX™ Test Equipment

Conformance test ensures interoperability with other WiMAX equipment and a positive end-user experience for your customers. With Keysight’s suite of WiMAX test equipment solutions, built on proven platforms, you can approach interoperability and conformance testing with very high confidence.

Protocol Conformance Test (PCT)
Keysight’s N6430A family of IEEE 802.16-2004/Cor2 D3 Protocol Conformance Test (PCT) solutions are based on the Keysight E6651A Mobile WiMAX™ Test Set. The N6430A product family provides protocol designers with a TTCN-3 scripting interface which supports script development for design needs, as well as the ability to run the ETSI validated protocol test cases in accordance with the WiMAX Forum® PCT certification requirements. http://www.keysight.com/find/pct

Network Conformance Test (NCT)
The N6434A Network Conformance Test (NCT) system provides a validated test regime for TTCN-3 network conformance testing. It can be used standalone or NCT test cases can be added to existing PCT solutions, since they use the same test infrastructure. This functionality offers users increased coverage of the comprehensive WiMAX certification test program. www.keysight.com/find/nct

Radiated Performance Test (RPT)
The E6651A is also used in radiated performance test (RPT) systems. RPT is undergoing evaluation to become part of the WiMAX Forum’s product certification process. Keysight’s WiMAX equipment, used by ETS-Lindgren in its AMS-8500 RPT system, enables these RPT measurements to be made and helps assure customers of their product quality. For more information visit WiMAXRPT at www.wimaxrpt.com 

Radio Conformance Test (RCT)
Keysight’s range of WiMAX equipment incorporates the latest industry-required measurements and are found in the AT4 Wireless MINT RCT System. WiMAX Forum Certified™ tests conformance and interoperability of WiMAX base station and subscriber-station products. AT4 Wireless is a WiMAX Forum designated certification laboratory. For more information visit AT4 Wireless at www.at4wireless.com/web_eng/systems/technologies/wimax.html

1-25 of 51

Sort:
N9075A & W9075A 802.16 OFDMA X-Series Measurement Application - Technical Overview 
The Mobile WiMAX measurement application transforms the X-Series signal analyzers into standard-based Mobile WiMAX transmitter testers by adding fast 1-button power and modulation measurements.

Technical Overview 2014-05-21

Wave 2 Mobile WiMax™ Measurements 89600 Vector Signal Analysis Software 
This demonstration guide provides step by step instructions for making Wave 2 Mobile WiMax™ measurements using the 89600 VSA software.

Demo 2011-03-05

PDF PDF 1.25 MB
Agilent Technologies Recognized for Leadership in LTE and WiMAX™ Test Equipment Market  

Press Materials 2009-12-15

 
2009 World Market Share Leadership Award by Frost & Sullivan 
Frost & Sullivan Recognizes Agilent Technologies for its Dominance of the WiMAX and LTE Test Equipment Market

Press Materials 2009-12-09

 
Agilent Technologies Equipment Used to Test First Mobile WiMAX Forum®-Certified Products in China La 

Press Materials 2009-08-31

 
89600 VSA Software Mobile WiMAX™ and Fixed WiMAX 
This two page flyer describes the 89600 Series vector signal analysis software WiMAX. Option B7Y OFDMA (mobile WiMAX) and Option B7S OFDM (fixed WiMAX). These options provide modulation analysis for WiMAX PHY layer signal problems.

Promotional Materials 2009-06-10

PDF PDF 155 KB
E6651A Mobile WiMAX™ Test Set - Technical Overview 

Technical Overview 2009-05-07

Agilent Technologies Announces New Functional Test Features for its E6651A Mobile WiMAX™ Test Set Fa 

Press Materials 2009-04-28

 
N6430A WiMAX Protocol Conformance Test and Development Solution - Technical Overview 

Technical Overview 2009-04-06

PDF PDF 942 KB
N9074A Single Acquisition Combined Fixed WiMAX X-Series Measurement Application Technical Overview 
The N9074A Single Acquisition Combined Fixed WiMAX X-Series measurement application. For use in the X-Series signal analyzers (MXA/EXA)

Technical Overview 2009-03-23

PDF PDF 770 KB
What Every RF Engineer Should Know: OFDM & WiMax 
Feature story by Janine Love.

Case Study 2008-12-27

 
An Overview of WiMAX™ Radiated Performance Test Requirements 
Published with kind permission of Communications Today

Article 2008-12-01

PDF PDF 292 KB
Mobile WiMAX™ Test Set Solutions Brochure 

Brochure 2008-10-21

PDF PDF 1.67 MB
Agilent Technologies' New PXB MIMO Receiver Tester Transforms MIMO Test for R&D Engineers 

Press Materials 2008-10-01

 
Agilent Technologies to Demonstrate Comprehensive Lineup of Fixed, Mobile WiMAX™ Test Solutions a 

Press Materials 2008-10-01

 
Agilent Technologies, Altair Semiconductor to Help Manufacturers Speed Development of Mobile WiMAX™ 

Press Materials 2008-09-29

 
Agilent Technologies' Firmware Update for its Mobile WiMAX™ Test Set Enables Faster Data  

Press Materials 2008-09-25

 
Power Accuracy in Receiver Test 
This application note tells how power measurement inaccuracy affects receiver tests, and shows you how to use external variable attenuators to increase accuracy and speed.

Application Note 2008-07-09

Agilent Technologies to Demonstrate WiMAX™ Test Solutions at 2008 Europe WIMAX Forum(r) Congress 

Press Materials 2008-06-17

 
Agilent Technologies Wins Contract from Sequans Communications for Mobile WiMAX(tm) Protocol Conform 

Press Materials 2008-06-10

 
Agilent Technologies Wins Contract from Bureau Veritas ADT for Mobile WiMAX™ PCT 

Press Materials 2008-04-09

 
Agilent Technologies to Demonstrate WiMAX™ Test Solutions at 2008 Asia WIMAX Forum(r) Congress 

Press Materials 2008-04-09

 
Agilent Technologies and NextWave Wireless Accelerate Mobile WiMAX™ Device Production, Deployment 

Press Materials 2008-04-02

 
Agilent Technologies and Runcom Technologies to Collaborate on Wave 2 Mobile WiMAX™ Protocol Test 

Press Materials 2008-02-11

 
Agilent Technologies Automates UMTS Cellular Mobile Stress Test with New Interactive Functional  

Press Materials 2008-01-15

 

1 2 3 Next