Contact an Expert

Verification, Integration, Protocol and Conformance of LTE Equipment

New component, base station, network and handset designs must meet the standards expected by the consumer—not to mention those required by industry bodies such as the GCF or PTCRB—and that means carrying out earlier and more comprehensive development, design verification and regression testing. In order to achieve this goal, versatile but rigorous test solutions are required. Keysight test equipment can validate LTE designs from pre-silicon protocol module development through system integration and verification.

Explore YouTube Videos 

1-25 of 48

Sort:
E7515A UXM Wireless Test Set - Brochure 
The UXM is a highly-integrated signaling test set for functional and RF design validation in the 4G era and beyond, so you can assess design readiness with greater confidence and make a clear call.

Brochure 2015-05-20

PDF PDF 2.77 MB
E7515A UXM Wireless Test Set - Flyer 
The UXM is a highly integrated signaling test set created for functional & RF design validation in the 4G era & beyond. It delivers LTE-A cat 6 now & will handle increasingly complex cases later.

Promotional Materials 2015-05-19

PDF PDF 1.56 MB
Keysight Demonstrates LTE-Advanced Category 11 IP Data Throughput with UXM Wireless Test Set 
Keysight announced verification of end-to-end IP data throughput for downlink rates of 587.5 Mbps with the E7515A UXM wireless test set. Using three component carriers (3CC) and 256 QAM in the downlink, Keysight achieved sustained bi-directional 3GPP UE category 11 data rates.

Press Materials 2015-05-06

 
N9080A/W9080A LTE FDD & N9082A/W9082A LTE TDD X-Series Application - Technical Overview 
An overview of the LTE FDD/TDD (N/W9080A & N/W9082A) X-Series measurement applications.

Technical Overview 2015-04-04

Keysight to Demonstrate New UXM Wireless Test Set Features at Mobile World Congress 
The E7515A UXM wireless test set is the industry’s leading UE test platform ready for 3CC/4CC, 256 QAM, UE categories 11-14. Visit us at Hall 2, Booth 212.

Press Materials 2015-02-12

 
Keysight Extends UXM Wireless Test Set LTE-A Carrier Aggregation Support with 3CC, TDD, Uplink  
The E7515A UXM wireless test set adds features to address the rapidly evolving 3GPP LTE-Advanced carrier aggregation advancements.

Press Materials 2015-01-21

 
Keysight Demonstrates LTE-A 450 Mbps End-to-End IP Data Throughput with UXM 
The E7515A UXM wireless test set provides verification of three component carrier (3CC) end-to-end IP data throughput.

Press Materials 2014-11-18

 
Agilent’s UXM Wireless Test Set Enables New Insights into LTE-Advanced Category 6 Chipsets, Devices 
Introducing the E7515A UXM wireless test set, the most highly integrated signaling test set created for functional and RF design validation in the 4G era and beyond.

Press Materials 2014-02-13

 
UXM Wireless Test Set Demo Videos on YouTube 
Explore YouTube for videos of the UXM wireless test set

Demo 2014-02-13

 
Greater Insight into LTE Design and Test 
This brochure discusses Keysight's leadership in LTE and presents our set of design and test solutions for LTE - from design simulation to signal generation and analysis through manufacturing and deployment.

Brochure 2013-12-31

PDF PDF 2.11 MB
Learn about LTE and its measurements in the LTE book written by 42 LTE experts 
Keysight’s new Long Term Evolution (LTE) book delves into the new 3GPP LTE cellular technology and offers tips for design, test and required equipment.

Promotional Materials 2013-01-24

 
Greater insight. Greater confidence. Accelerate next-generation wireless - Brochure 
This brochure speaks to Keysight's Cellular from products, to experts to knowledge library and how Keysight gives you greater insight and greater confidence into Cellular.

Brochure 2012-05-31

PDF PDF 1.11 MB
Agilent Technologies Announces Voice-over-LTE Test System Developed with Brüel & Kjær 
Transporting voice over a packet-based LTE cellular infrastructure poses challenges that make voice-quality testing essential. The Agilent and Brüel & Kjær solution combines standards-based test methods with real-world base station emulation, RF test and functional test to ensure that VoLTE phones will meet user's expectations.

Press Materials 2012-05-10

 
Agilent Technologies Introduces 6-GHz Signal Generators with Industry-Best Performance 
Today's aerospace/defense environment requires enhanced radar performance to detect weak signals at long distances. To provide the pure and precise signals needed to test these designs, the MXG uses an innovative triple-loop synthesizer to deliver phase noise performance of -146 dBc/Hz at 1 GHz and 20 kHz offset. For developers of radar components such as mixers and analog-to-digital converters, the MXG also features industry-leading spurious performance of -96 dBc at 1 GHz.

Press Materials 2012-05-01

 
ETS-Lindgren Announces Support of Agilent PXT Wireless Test Set for LTE Over-the-Air Testing 
Agilent PXT performs OTA tests to industry standards and allows user equipment (UE) developers to characterize and optimize the behaviour of their designs. The EMQuest/PXT solution is offered with all ETS-Lindgren AMS for the testing of wireless devices

Press Materials 2012-02-03

 
Agilent Technologies Announces Industry's First Eight-Channel RF Measurement Solution Addressing LTE 
Agilent Technologies Inc. (NYSE: A) today introduced industry-leading enhancements to its N7109A multi-channel signal analyzer for emerging multichannel LTE, LTE-Advanced and MIMO RF measurement requirements, including LTE antenna beamforming and LTE-Advanced carrier aggregation.

Press Materials 2012-02-02

 
Agilent Technologies Announces Bluetest Support of Agilent PXT for LTE Over-the-Air Testin 
Agilent Technologies Inc. (NYSE: A) today announced that Bluetest AB now supports Agilent's PXT wireless communications test set. The Bluetest RTS (Reverberation Test System) uses the Agilent PXT test set to evaluate LTE devices over the air.

Press Materials 2012-02-02

 
Testing Handovers Between LTE and 3G cdma2000/1xEV-DO Cellular Networks - Application Note 
This application note explains test handovers between LTE and third generation cdma2000/1xEV-DO cellular networks as well as network evolution.

Application Note 2011-06-15

89601B/BN-BHD LTE FDD Modulation Analysis, 89600 VSA Software - Demo Guide 
This demonstration guide provides step by step instructions for making 3GPP LTE measurements using the 89600 VSA software.

Demo 2011-02-23

PXT Wireless Communications Test Set (E6621A) - Application Note 
This application note provides you with the basic steps to making data throughput measurements with your E6621A PXT.

Application Note 2011-02-04

P-Series Power Meter/Sensor LTE Measurement 
This article covers the technical overview and features, benefits and specifications of the P-Series power meters and sensors for LTE-TDD measurement applications.

Technical Overview 2010-11-19

Agilent Technologies and Nomor Research GmbH Generate LTE Uplink Inter-cell Interference Signals 
Agilent Technologies Inc. (NYSE: A) and Nomor Research GmbH today announced the availability of a simple, cost-effective method for generating realistic LTE uplink inter-cell interference signals using Agilent's MXG signal generators.

Press Materials 2010-10-22

 
YouTube Video: LTE Master and System Information Block Recovery 
This is a demonstration of how the master information block and system information blocks can be recovered from the LTE downlink signal using the Keysight 89600 VSA signal analysis software.(YouTube video, 5:53min)

Demo 2010-09-24

 
LTE eNB Closed-loop Conformance Testing 
This is a demonstration of how the Keysight N5106A PXB baseband generator and channel emulator, N7624B Signal Studio for LTE software, and N5182A MXG signal generator are configured for eNB closed-loop conformance test. (8.27min)

Demo 2010-09-24

 
YouTube video: LTE 5MHz Downlink signal demonstrated on a Keysight VSA 89600 
View an LTE downlink signal then watch it being demodulated and decoded for further analysis. (YouTube video, 5 min)

Demo 2010-09-24

 

1 2 Next