Contact an Expert

Femtocell Test

As a world leader in test and measurement solutions, Keysight continues to be at the forefront of emerging markets such as small-cell base stations. Femtocells are small-cell base stations typically designed for indoor use in residential or small business environments. They connect to a service provider’s network via the end user’s broadband internet. As small cells gain momentum, keeping pace with growing demand and aggressive schedules is easier when you have access to deeper resources. From R&D through manufacturing, Keysight has femtocell test equipment available now to help you meet your time to market goals. The EXF is the industry’s first one-box tester dedicated to femtocell manufacturing, and it’s validated with the latest cellular and WLAN chipsets. Access our expertise in base-station and high-volume testing and accelerate femtocell manufacturing with the EXF.

Explore YouTube Videos 

1-18 of 18

E6650A EXF Wireless Test Set for Femtocell - Flyer 
The E6650A EXF is the industry's first one-box tester dedicated to femtocell manufacturing and it is validated with the latest cellular and WLAN chipsets.

Promotional Materials 2014-09-10

Solutions and Measurement Tools for Use in Average Power and Envelope Tracking Design - Application  
This app note provides an outline of the techniques involved and the solutions Agilent provides for RF, baseband and system developers.

Application Note 2014-08-02

Agilent Technologies Introduces 6-GHz Signal Generators with Industry-Best Performance 
Today's aerospace/defense environment requires enhanced radar performance to detect weak signals at long distances. To provide the pure and precise signals needed to test these designs, the MXG uses an innovative triple-loop synthesizer to deliver phase noise performance of -146 dBc/Hz at 1 GHz and 20 kHz offset. For developers of radar components such as mixers and analog-to-digital converters, the MXG also features industry-leading spurious performance of -96 dBc at 1 GHz.

Press Materials 2012-05-01

Designing and Testing 3GPP W-CDMA Base Stations (Including Femtocells) - Application Note 
W-CDMA is one of several wideband digital cellular technologies competing for the third-generation (3G) cellular market.

Application Note 2010-08-01

Test your Femtocells Today 
This photo card includes the key measurements required for femtocell designs as well as Keysight's portfolio of design and test solutions for femtocell technology.

Brochure 2010-07-01

Agilent Technologies Supports Percello's Femtocell SoCs Test with Chipset Software 
Agilent Technologies Inc. (NYSE: A) announced its N7309A chipset software now supports high-volume manufacturing test for Percello's Aquilo Femtocell System-on-a-Chip (SoC) product line.

Press Materials 2010-06-16

Agilent Technologies Chipset Software Supports picoChip Femtocell Test 
Agilent Technologies Inc. (NYSE: A) and picoChip today announced a high-volume manufacturing test solution for 3G femtocell products.

Press Materials 2010-06-08

W-CDMA BER Test on picoChip Femtocell Reference Design Using Keysight MXG  
This application note explains single-direction BER testing of femtocell devices based on picoChip femtocell reference designs using the Keysight N5182A MXG vector signal generator.

Application Note 2009-12-15

3GPP Long Term Evolution: System Overview, Product Development and Test Challenges -Application Note 
This application note focuses on LTE and includes content on system overview, product development and test challenges of this new wireless communications technology.

Application Note 2009-09-08

Solutions for Femtocell Manufacturing Test 
This short application brief discusses how to best accelerate the delivery of quality, low-cost femtocells to market.

Application Note 2009-05-05

Techniques and Trends in Signal Monitoring, Frequency Management and Geolocation of Wireless 
This application note reviews various issues, techniques and associated equipment required for signal monitoring and frequency management of RF spectrum in the VHF/UHF frequency range.

Application Note 2009-04-27

GPS: making a play for femtocells 
This article from Microwave Engineering Europe Jan/Feb 2009 discusses the issues that arise when integrating GPS into femtocells and outlines the test and verification requirements that this introduces.

Article 2009-04-16

Agilent Technologies First to Extend Real-Time Wireless Network Protocol Analysis to Support Femtoce 

Press Materials 2009-03-30

Agilent Technologies, ASTRI, PicoChip Demonstrate Design and Test of TD-LTE Femtocell at 2009 Mobile 

Press Materials 2009-02-16

Agilent Technologies to Display Newest Mobile Communications Test, Measurement Solutions at 2009 Mob 

Press Materials 2009-02-02

Agilent Technologies Displays Comprehensive Femtocell Testing Capability 

Press Materials 2008-12-01

Expert Advice: The Importance of Average vs. Peak Performance in Cellular Wireless 
The average efficiency of the cell remains much lower than the peaks. November 2008 article by Moray Rumney linked with permission by Microwave Journal.

Article 2008-11-17

Agilent Technologies, picoChip, mimoOn Demonstrate 3GPP LTE Femtocell Testing Capability 

Press Materials 2008-07-22