Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

Installation & Maintenance of LTE Equipment

Customers demand uninterrupted quality service. That means technicians must rapidly detect and diagnose equipment problems and detect and identify unknown signals. Additionally, networks span varied environments and technologies. Keysight field-ready test equipment means you can increase productivity and boost your readiness. For LTE testing, one-button GSM/WCDMA/LTE power measurements make Node B transmitter tests much easier and worry free. LTE TDD spectrum analysis power measurement enables identification of uplink interference during network operation.

Explorer les vidéos YouTube 

1-22 sur 22

Tri:
Correlating Microwave Measurements between Handheld and Benchtop Analyzers - Application Note 
This application note discusses the powerful capabilities of modern-day handheld analyzers and includes measurement comparisons between FieldFox handheld analyzers and several benchtop instruments.

Notes d’application 2015-08-27

Precision Validation, Maintenance and Repair of Satellite Earth Stations FieldFox Handheld Analyzers 
This application note describes breakthrough technologies that have transformed the way systems can be tested in the field while providing higher performance, improved accuracy and capability.

Notes d’application 2015-08-24

Techniques for Precise Measurement Calibrations in the Field - Application Note 
This application note discusses recent advances in VNA calibration and compares measurements made on a FieldFox analyzer using different calibration types for a variety of RF and microwave devices.

Notes d’application 2015-05-22

Techniques for Precise Cable and Antenna Measurements in the Field - Application Note 
This app note introduces measurement and calibration techniques for cable and antenna testing using FieldFox handheld analyzers.

Notes d’application 2015-05-15

Techniques for Precise Interference Measurements in the Field - Application Note 
This app note discusses the different types of interference in current and new systems and methods to measure a variety of interference types using spectrum analyzers such the FieldFox Series.

Notes d’application 2015-03-30

Greater Insight into LTE Design and Test 
This brochure discusses Keysight's leadership in LTE and presents our set of design and test solutions for LTE - from design simulation to signal generation and analysis through manufacturing and deployment.

Brochure 2013-12-31

PDF PDF 2.11 MB
Learn about LTE and its measurements in the LTE book written by 42 LTE experts 
Keysight’s new Long Term Evolution (LTE) book delves into the new 3GPP LTE cellular technology and offers tips for design, test and required equipment.

Matériel de promotion 2013-01-24

 
Agilent Technologies Enhances FieldFox RF Analyzers with Options for Measuring Time Domains and Chan 
Agilent will demonstrate its new FieldFox options, along with solutions that cover everything from circuit-level modeling through system verification for general RF, microwave, 4G communications, and aerospace/defense applications at IMS 2012/IEEE MTT-S (Booth 1015), June 19-21, in Montr�al, Canada. A range of premier partner solutions will also be available on Agilent Avenue and throughout the event area.

Dossier de presse 2012-05-01

 
Learn about 3GPP LTE and other Cellular technologies with these useful resources 
Order posters, CDs and more. Download many application notes and brochures and view videos.

Matériel de promotion 2011-11-17

 
Interference Testing with Handheld Spectrum Analyzers - Application Note 
This application note describes the techniques and procedures for interference testing in a wireless environment using the Keysight family of N934xC/N9340B handheld spectrum analyzers.

Notes d’application 2011-10-11

LTE-Advanced…Already? 
Article reprint from OSP magazine detailing the additional changes LTE-Advanced brings to the Network already working to implement 3GPP LTE.

Article 2011-09-01

PDF PDF 695 KB
Testing Handovers Between LTE and 3G cdma2000/1xEV-DO Cellular Networks - Application Note 
This application note explains test handovers between LTE and third generation cdma2000/1xEV-DO cellular networks as well as network evolution.

Notes d’application 2011-06-15

Move Forward to What's Possible in TD-LTE-Design & Test Solutions 
This brochure focuses on Keysight's design and test solutions for TD-LTE including design simulation, signal generation & analysis, baseband analysis, validation and network optimization solutions.

Brochure 2009-12-24

PDF PDF 1.56 MB
LTE Solutions in Network Deployment and Optimization 
Keysight’s E6474A and N9912A provide air interface troubleshooting and optimization, cell site test and interference hunting on LTE systems

Présentation technique 2009-11-13

PDF PDF 242 KB
Agilent Technologies to Show Latest LTE Test Solutions at LTE Americas 2009 

Dossier de presse 2009-11-02

 
3GPP Long Term Evolution: System Overview, Product Development and Test Challenges -Application Note 
This application note focuses on LTE and includes content on system overview, product development and test challenges of this new wireless communications technology.

Notes d’application 2009-09-08

Agilent Technologies Now Offers Most Comprehensive Real-Time Diagnostics, Analysis for LTE 

Dossier de presse 2009-02-16

 
Agilent Technologies' New Drive Test Measurements Speed Deployment, Cut Costs of LTE Networks 

Dossier de presse 2009-02-02

 
Agilent Technologies to Display Newest Mobile Communications Test, Measurement Solutions at 2009 Mob 

Dossier de presse 2009-02-02

 
Analyze Antenna Approaches for LTE Wireless Systems 
Multiple-antenna techniques are a large part of improved performance in LTE wireless systems, but they must be properly understood in order to be properly tested.

Article 2008-08-13

 
LTE ARQ and Re-segmentation 
Link to August 2008 Microwave Journal Article

Article 2008-08-08

 
3GPP LTE: Introducing Single-Carrier FDMA  
This article, published in issue 4 of the Agilent Measurement Journal, describes single-carrier FDMA for 3GPP LTE.

Article 2008-01-01

PDF PDF 491 KB