这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

LTE 的网络部署和服务保证

查看相关视频(优酷) 

1-21 / 21

排序:
是德科技手持式分析仪与台式分析仪的微波测量功能对比 
是德科技手持式分析仪与台式分析仪的微波测量功能对比

应用说明 2016-05-30

在现场执行精密干扰测量的技巧 使用 FieldFox 手持式分析仪 
在现场执行精密干扰测量的技巧 使用 FieldFox 手持式分析仪

应用说明 2014-09-12

在现场执行精密电缆和天线测量的技巧 使用 FieldFox 手持式分析仪 
在现场执行精密电缆和天线测量的技巧 使用 FieldFox 手持式分析仪

应用说明 2014-09-12

在外场执行精密测量校准的技巧 使用 FieldFox 手持式分析仪 
在外场执行精密测量校准的技巧 使用 FieldFox 手持式分析仪

应用说明 2014-08-06

阅读 42 位 LTE 专家共同倾力撰写的 LTE 著作,了解 LTE 的历史背景与最新发展及相关测量 
是德科技发布关于长期演进(LTE)的最新著作,对 3GPP LTE 蜂窝新技术进行了深入分析,并提供了各种设计和测试技巧,以及必要的设备。

促销资料 2013-01-24

 
Agilent Technologies Enhances FieldFox RF Analyzers with Options for Measuring Time Domains and Chan 
Agilent will demonstrate its new FieldFox options, along with solutions that cover everything from circuit-level modeling through system verification for general RF, microwave, 4G communications, and aerospace/defense applications at IMS 2012/IEEE MTT-S (Booth 1015), June 19-21, in Montr�al, Canada. A range of premier partner solutions will also be available on Agilent Avenue and throughout the event area.

新闻资料 2012-05-01

 
利用是德的重要资源了解 3GPP LTE 和其他无线技术 
订购“了解 LTE 的复杂性”宣传海报或光盘以及其他材料

促销资料 2011-11-17

 
根据手持式频谱分析仪应用指南进行干扰测试 
This application note describes the techniques and procedures for interference testing in a wireless environment using the Keysight family of N934xC/N9340B handheld spectrum analyzers.

应用说明 2011-10-11

LTE-Advanced…Already? 
Article reprint from OSP magazine detailing the additional changes LTE-Advanced brings to the Network already working to implement 3GPP LTE.

文章 2011-09-01

PDF PDF 695 KB
测试 LTE 和 3G cdma2000/1xEV-DO 蜂窝式网络技术间的切换 
This application note explains test handovers between LTE and third generation cdma2000/1xEV-DO cellular networks as well as network evolution.

应用说明 2011-06-15

通过 30 位 LTE 专家携手编写的最新 LTE 专著了解 LTE 及其测量 
Keysight’s new Long Term Evolution (LTE) book delves into the new 3GPP LTE cellular technology and offers tips for design, test and required equipment.

促销资料 2010-11-15

 
Move Forward to What's Possible in TD-LTE-Design & Test Solutions 
This brochure focuses on Keysight's design and test solutions for TD-LTE including design simulation, signal generation & analysis, baseband analysis, validation and network optimization solutions.

手册 2009-12-24

PDF PDF 1.56 MB
LTE Solutions in Network Deployment and Optimization 
Keysight’s E6474A and N9912A provide air interface troubleshooting and optimization, cell site test and interference hunting on LTE systems

技术总览 2009-11-13

PDF PDF 242 KB
Agilent Technologies to Show Latest LTE Test Solutions at LTE Americas 2009 

新闻资料 2009-11-02

 
3GPP Long Term Evolution: System Overview, Product Development and Test Challenges -Application Note 
This application note focuses on LTE and includes content on system overview, product development and test challenges of this new wireless communications technology.

应用说明 2009-09-08

Agilent Technologies Now Offers Most Comprehensive Real-Time Diagnostics, Analysis for LTE 

新闻资料 2009-02-16

 
Agilent Technologies' New Drive Test Measurements Speed Deployment, Cut Costs of LTE Networks 

新闻资料 2009-02-02

 
推动LTE 的创新和发展 
推动LTE 的创新和发展

手册 2009-01-01

PDF PDF 2.73 MB
Analyze Antenna Approaches for LTE Wireless Systems 
Multiple-antenna techniques are a large part of improved performance in LTE wireless systems, but they must be properly understood in order to be properly tested.

文章 2008-08-13

 
LTE ARQ and Re-segmentation 
Link to August 2008 Microwave Journal Article

文章 2008-08-08

 
3GPP LTE: Introducing Single-Carrier FDMA  
This article, published in issue 4 of the Agilent Measurement Journal, describes single-carrier FDMA for 3GPP LTE.

文章 2008-01-01

PDF PDF 491 KB