您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

WLAN 802.11ac 測試與設計

802.11ac 是最新的 WLAN 標準,它建構於 802.11n 之上,但具備高達 160 MHz 的射頻頻寬、MIMO,以及高密度 256QAM 調變信號, 使其得以在低於6 GHz的頻段中,為多個無線存取裝置提供每秒 1 Gigabit 的傳輸速率。 Keysight 802.11ac 軟體可部署於元件和接收器中,方便使工程師查看所有的 802.11ac 調變格式並進行故障診斷(從 BPSK 到 256QAM)。 為獲得更高的靈活性,該軟體支援所有的信號頻寬,包括 20、40、80 和 160 MHz,同時還支援高達 4x4 的 MIMO。 搭配 Keysight 89600B VSA 802.11ac 軟體使用時,無論工程師採用的是哪種 802.11ac 格式,皆可更深入分析新一代的 802.11ac WLAN 晶片和裝置。 清楚洞察、 信心滿滿。 加速開發新世代無線裝置

欲深入了解 WLAN,請查看 WLAN 資源


 

觀看YouTube影片 

1-21 / 21

排序:
Testing New-Generation WLAN 802.11ac - Application Note 
This application note introduces the new WLAN new-generation testing technology of 802.11ac and the many different Keysight solutions for testing WLAN 802.11ac.

應用手冊 2015-04-01

E6640A EXM Wireless Test Set Ready for Volume Production of LTE-A, 802.11ac WLAN Devices 
Agilent Technologies today announced the E6640A EXM wireless test set, which offers breakthrough manufacturing-test scalability in technology coverage, performance and capacity to test up to 32 cellular and wireless-connectivity devices in parallel.

新聞資料 2014-02-13

 
E6640A EXM 無線測試儀 - 配置指南 
E6640A EXM 無線測試儀 - 配置指南

配置設定指南 2013-12-09

Creating and Optimizing 802.11ac Signals with the M8190A AWG - Application Note 
Designs for 802.11ac WLAN devices require test equipment that can provide the best reference test signals and measurements. N7617B enables this type of signals to be generated with the M8190A AWG.

應用手冊 2013-08-13

PDF PDF 606 KB
What is the difference between IEEE 802.11ac and 802.11ad? 
Microwave & RF article, April 2013. The goal is for all IEEE 802.11 standards to be backward compatible and for 802.11ac and 802.11ad to be compatible at the medium-access-control (MAC) or data-link layer. They should differ only in physical-layer (PHY) characteristics. Read about how that goal is being attained.

專文 2013-04-23

 
Multichannel Measurements in MIMO 802.11ac Baseband IQ Simulation, Design & Test - Application Note 
This solution brief will show Keysight Technologies' complete, end-to-end solution for multichannel measurements of 802.11ac BBIQ simulation, design and test.

應用手冊 2013-04-05

PDF PDF 748 KB
Agilent Technologies Releases New Software for X-Series Signal Analyzers 
Agilent Technologies extended its leadership in 802.11ac WLAN test solutions with its latest measurement application release for X-Series signal analyzers. The software release offers expanded WLAN support to include the emerging 802.11ac standard.

新聞資料 2012-11-01

 
802.11ac Power Measurement and Timing Analysis - Application Note 
This technical article illustrates how Keysight 8990B peak power analyzer able to help technicians and engineers perform some of the test requirements when developing 802.11ac power amplifier module

應用手冊 2012-09-02

PDF PDF 3.46 MB
Creating and Optimizing 802.11ac Signals Application Note 
This application note details how to create and optimize 802.11ac signals using the N7617B Signal Studio for WLAN 802.11a/b/g/n/ac software with Keysight's RF signal generators to get the highest quality signals from the instruments.

應用手冊 2012-07-19

PDF PDF 2.10 MB
Agilent Technologies Introduces 6-GHz Signal Generators with Industry-Best Performance 
Today's aerospace/defense environment requires enhanced radar performance to detect weak signals at long distances. To provide the pure and precise signals needed to test these designs, the MXG uses an innovative triple-loop synthesizer to deliver phase noise performance of -146 dBc/Hz at 1 GHz and 20 kHz offset. For developers of radar components such as mixers and analog-to-digital converters, the MXG also features industry-leading spurious performance of -96 dBc at 1 GHz.

新聞資料 2012-05-01

 
Tackling MIMO Design and Test Challenges for 802.11ac WLAN 
This article from Microwave Journal shows how the system engineer can use system simulation to help understand the design performance and design requirements needed to achieve transmitter system-level metrics such as EVM.

專文 2012-03-11

 
Agilent Technologies Introduces Innovative Multi-Measurement Signal Analyzer Capability for Wireless 
Agilent Technologies Inc. (NYSE:A) today announced that an innovative, new multi-measurement capability is being added to its 89600 VSA software, enabling simultaneous signal analysis of multiple carriers and signal formats for more efficient testing and deeper signal insight in wireless test.

新聞資料 2011-11-15

 
802.11ac Wireless LAN: what’s new and the impact on design and test 
EE times article by Agilent’s Mirin Lew describing the 802.11ac, the technical challenges and comparisons to earlier technologies.

專文 2011-11-09

 
Agilent Technologies' PXA Signal Analyzer Now Enables Wideband Measurement with up to 900  
Agilent Technologies Inc. (NYSE:A) today announced that its high-performance PXA signal analyzer now supports up to 900 MHz of intermediate-frequency bandwidth, enabling it to act as a broadband down converter for analysis of wideband communications and radar signals in aerospace and defense applications.

新聞資料 2011-09-20

 
Agilent Technologies Announces Industry's First 160-MHz Signal Analyzer for Wide Bandwidth Signal 
The PXA's 160-MHz bandwidth enables the wider bandwidth signal analysis that today's engineers demand

新聞資料 2011-09-19

 
Agilent Technologies Introduces Wideband DPD Modeling Platform for LTE-Advanced, 802.11ac  
Agilent Technologies Inc. (NYSE: A) today announced the newest release of its W1716 Digital Pre-Distortion Builder (DPD) software, designed to enable the high levels of wireless performance necessary for emerging wideband standards such as LTE-Advanced and IEEE 802.11ac.

新聞資料 2011-08-31

 
Agilent Extends Wireless Leadership with First-To-Market Support for 802.11ac Design and Analysis 
Agilent Technologies announces that its 89600B vector signal analysis software is now able to test 802.11ac signals. This is the first dedicated 802.11ac signal analysis solution on the market.

新聞資料 2011-03-17

 
Custom OFDM Signal Generation Using SystemVue - Application Note 
This application note describes a new comms standard based on OFDM which is provided by SystemVue 2011 to create both simulation and measurement, with links to the new 89600B VSA software for further demodulation and analysis.

應用手冊 2010-12-09

Caution: MIMO Test Challenges Ahead 
Article published by Wireless Design & Development on MIMO testing challenges and methods to achieve higher data rates such as two0 and four-channel MIMO.

專文 2010-09-20

PDF PDF 70 KB
MIMO Wireless LAN PHY Layer (RF) Operation & Measurement Application Note 1509 
This application note is intended to provide an understanding of MIMO radio operation as it applies to WLAN, and the test configurations for multi-channel radios.

應用手冊 2008-04-30

Equalization Techniques and OFDM Troubleshooting for Wireless LANs - AN 1455 
The discussions and measurements described here apply most specifically to the Keysight 89600 Series vector signal analyzers and their wireless networking measurement software.

應用手冊 2003-05-07