Contact an Expert

RF & Microwave Design

Keysight design software provides proven RF and Microwave solutions with very accurate models and powerful simulation technologies ranging from circuit, electromagnetic (EM), and system level designs. With Keysight, you'll be equipped to pinpoint, optimize and deliver - on time.

RF and Microwave Design Challenges

  • Ever increasing substrate layer counts, smaller form factors, complex packaging technologies, and closer design proximities continue to make designs ever more challenging
  • Seamlessly integrated circuit and EM simulation tools that flow from schematic entry through to production and verification
  • Continuous innovation of simulation technology performance to increase accuracy while dramatically reducing simulation speeds

Explore YouTube Videos 

1-25 of 210

Sort:
How to Design an RF Power Amplifier: Class E 
This video provides an introduction to Class E Power Amplifiers and demonstrates a superior, time saving methodology to design and practically realize a Class E RF power amplifier using first principles to build an ideal circuit and then utilizing circuit design tools to synthesize a more realistic circuit topology from the ideal case.

How-To Video 2015-03-11

 
Keysight Technologies to Demonstrate Latest EMC Design, Test Tools at EMCSI Symposium 
Keysight announces it will demonstrate and discuss the latest tools and techniques on 1) EMC design and testing, and 2) signal and power integrity at the EMCSI 2015 Symposium, Santa Clara Convention Center, Booth 618, March 17-19.

Press Materials 2015-03-09

 
Keysight EEsof EDA Newsletter - Product and Application News 
Keep tabs on the latest product and application news and review the archives of the Keysight EEsof EDA Newsletter.

Newsletter 2015-03-04

 
How to Predict Package and Bondwire Effects on Your RF-Module Designs 
This short video shows how to predict package, board, and bond wire effects on your RF-module designs which subsequently enables you to fix the design prior going to fabrication. The video demonstrates the process of building modules that comprise different technologies and performing EM simulation on them.

How-To Video 2015-02-19

 
Genesys - Brochure 
12-page Genesys color brochure and configuration guide. Provides information to help with purchasing decisions and justifications.

Brochure 2015-02-15

PDF PDF 7.40 MB
M9068A Phase Noise X-Series Measurement Application for PXI Vector Signal Analyzers 
This document provides technical and other information related to the Phase Noise X-Series measurement application for modular instruments.

Technical Overview 2015-02-10

PDF PDF 2.39 MB
How to Use Envelope Tracking to Improve Power Amplifier Efficiency 
This video introduces basic concepts regarding applying envelope tracking to improve power amplifier efficiency.

How-To Video 2015-02-10

 
Recommendations for Port Setup When Using ADS Momentum and Modelithics Models 
This application note is intended to help Advanced Design System (ADS) users using Modelithics models, simulate RF & Microwave circuits. The focus is on finding the optimum port setup for EM simulation of circuit layouts that include surface-mount technology (SMT) devices.

Application Note 2015-02-05

PDF PDF 1.43 MB
How to Make Accurate, Automated RF Wafer-level Measurements 
The video introduces automation as a way to increase productivity and efficiency. Keysight WaferPro Express measurement software is used to illustrate the various steps in combination with Cascade Microtech Velox software for prober control and Cascade WinCalXE software for automated calibration.

How-To Video 2015-01-27

 
How to Design an RF Power Amplifier: Class F 
This short video will provide an introduction to Class F Power Amplifier Design by first building a nonlinear device model and then using this model in a circuit simulation environment to generate the idealized “square” Class F waveforms.

How-To Video 2015-01-27

 
How to Setup and Run Load Pull Simulations: The Basics 
This video introduces basic concepts regarding running load pull simulations. It then uses load pull simulation to find a load impedance that enables you to obtain greater than 43 dBm output power and greater than 55% PAE from a Cree FET.

How-To Video 2015-01-27

 
How to Design an RF Power Amplifier: The Basics  
This video provides a foundation for understanding how power amplifier circuits work. If you are new to High Frequency Power Amplifier Circuit Design, this is the place to start.

How-To Video 2015-01-15

 
How to Apply EM Port Calibration to Improve Simulation Accuracy (MoM) 
This video covers 5 different Momentum calibration methods and shows how the different types of calibration methods impact simulation results along with where and how to use them properly.

How-To Video 2015-01-15

 
How to Design an RF Power Amplifier: Class A, AB and B 
This video provides an introduction to the most basic modes of power amplifier operation by first building a nonlinear device model from scratch and then using this model in a circuit simulation environment to demonstrate various modes of power amplifier operation.

How-To Video 2015-01-15

 
How to Characterize and Optimize Connector to Board Transition Designs 
This video demonstrates how to accurately model an SMA to PCB transition to obtain agreement between simulated and measured results and how to improve the transition performance.

How-To Video 2015-01-15

 
How to Use “Design of Experiments” to Create Robust Designs With High Yield 
This video explains how to use the DOE methodology to help you create and produce robust designs with first pass success and high yield.

How-To Video 2015-01-14

 
How to Optimize the Performance of Your RF Layout 
This video shows a practical and effective approach to optimize the performance of your RF layout by parameterizing it and performing EM optimization prior to going to fabrication – thus helping to achieve fist pass success.

How-To Video 2015-01-14

 
How to Design RF and Microwave Impedance Matching Networks 
This video describes how to design RF and Microwave impedance matching networks.

How-To Video 2015-01-14

 
Keysight Technologies’ GoldenGate Software Release Delivers New and Enhanced Capabilities 
Keysight announces the latest release of GoldenGate software, the industry's most trusted and proven simulation, analysis and verification solution for large-scale RFIC circuit design.

Press Materials 2015-01-13

 
Keysight Unveils Silicon RFIC Interoperability in Latest Advanced Design System Software Release 
Keysight introduces the latest release of its powerful ADS software, ADS 2015. Featuring silicon RFIC interoperability with Cadence’s Virtuoso, GoldenGate-in-ADS, and a host of capabilities intended to increase design efficiency, the Keysight EEsof EDA software, ADS 2015, is changing how silicon RFIC and multi-technology module design is performed.

Press Materials 2015-01-06

 
Keysight Silicon RFIC Design Solutions 
In this video we show the Keysight Silicon RFIC design solutions that help you achieve your goals for designing today´s challenging RFICs and successfully going beyond the IC to verify its performance in higher levels of integration.

Demo 2015-01-05

 
Keysight Donates $120 Mil. Gift of Software, Support and Training to Georgia Institute of Technology 
Keysight announces the largest in-kind software donation in its longstanding relationship with the Georgia Institute of Technology.

Press Materials 2014-12-10

 
Keysight Receives Global Frost & Sullivan Award for Market Leadership in Instrumentation Software 
Keysight Technologies announces that Frost & Sullivan has recognized Keysight with the 2014 Global Frost & Sullivan Award for Market Leadership in Instrumentation Software for excellence in capturing the highest market revenue within its industry. The award is based on Frost & Sullivan's recent analysis of the instrumentation software market.

Press Materials 2014-12-08

 
Keysight Technologies Unveils Significant FEM Simulation Speed Increase in Latest 3-D EM Simulation  
Keysight announces the latest release of Electromagnetic Professional (EMPro) software, its 3-D electromagnetic simulation software.

Press Materials 2014-12-02

 
Accurate testing of the dielectric properties of powders, liquids and pliable materials – MWI Labora 
Accurate testing of the dielectric properties of powders, liquids and pliable materials – MWI Laboratories and Keysight

Solution Brief 2014-12-01

 

1 2 3 4 5 6 7 8 9 Next