这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

射频与微波设计

是德设计软件提供业经验证的射频和微波解决方案,这些解决方案具有极其精确的模型和功能强大的仿真技术,覆盖了电路、电磁场(EM)和系统级设计等方面。使用是德产品,您将可以精确查明问题所在,优化设计并按时交付。

射频和微波设计挑战

  • 不断增加的基片层数目、更小巧的外形、复杂的封装技术以及更好的设计接近性,这些因素使得设计更具挑战性。
  • 无缝集成电路和电磁场仿真工具能够覆盖从原理图输入到生产、验证的整个过程。
  • 仿真技术性能的不断创新在提高精度的同时,也会大幅降低仿真速度

查看相关视频(优酷) 

1-25 / 298

排序:
How to Estimate Voltage Spikes from Layout Parasitic Inductance in Switched-Mode Power Supplies 
We showed you how to deal with layout parasitic inductance in our previous video entitled “How to design DC-to-DC power converters”, but a frequently asked question was “When should I start to worry about layout parasitics inductance? Is there a quick rule of thumb that says kind of ‘Caution: Further investigation’s needed?’” The answer is yes and this follow up video is about how to make these estimates.

视频演示 2017-07-17

 
Keysight EEsof EDA Newsletter - Product and Application News 
Keep tabs on the latest product and application news and review the archives of the Keysight EEsof EDA Newsletter.

内部通讯 2017-07-07

 
Making Better Models with User Data 
This paper details the process of combining MATLAB and the RF System analysis to improve the accuracy of simulations via personalized models.

应用说明 2017-06-24

PDF PDF 1.44 MB
EDAcafé - DAC 2017 Interview: Michel Azarian, Silicon RFIC EDA Program Manager 
Sanjay Gangal from EDAcafé interviews Michel Azarian (Keysight Technologies' Silicon RFIC EDA Program Manager) at Design Automation Conference (DAC) 2017.

基本演示 2017-06-22

 
Keysight EEsof EDA SystemVue 
SystemVue is an EDA environment for electronic system-level (ESL) design that allows system architects and algorithm developers to innovate the physical layer (PHY) of communications systems.

技术总览 2017-06-21

Keysight Demonstrates Latest Design, Simulation, Verification Solutions at DAC 
Keysight Technologies will showcase the newest releases of its EDA software for RF-microwave circuit and system, high-speed digital, electronic system level, 3-D electromagnetic, and device-modeling applications at the 54th annual Design Automation Conference (www.dac.com), the premier conference for design and automation of electronic systems.

新闻资料 2017-06-14

 
Video Clips from the "Four Ways to Boost Simulation Data Processing using Python" Webcast 
Watch these powerful video clips from the Keysight webcast, "Four Ways to Boost Simulation Data Processing using Python".

基本演示 2017-06-12

 
Electrothermal Simulation using the Wolfspeed ADS PDK  
This is a short demonstration of how the Wolfspeed ADS PDK is configured to work with the ADS electrothermal simulator to co-simulate electrical and thermal performance. This allows designers to quickly understand the impact of thermal effects on their circuit designs, and account for those effects during the design process.

基本演示 2017-06-02

 
Keysight Technologies to Present a Vision for 5G Evolution at WAMICON 2017  
Keysight experts will be at WAMICON 2017, an annual IEEE Wireless and Microwave Conference, to discuss everything from circuit-level modeling to system verification for general RF, microwave, millimeter wave for 4G, emerging 5G communications, and aerospace & defense.

新闻资料 2017-04-10

 
M9421A VXT PXIe Vector Signal Transceiver - Configuration Guide 
This configuration guide contains information to configure the M9421A VXT PXIe vector transceiver

配置指南 2017-03-30

PDF PDF 1.91 MB
Electronic Components Tolerance and Test Limits for In-Circuit Test - Technical Overview 
In order for all assembled components to function correctly, components are measured and analyzed electrically using the In-circuit tester to ensure its value and performance are optimal.

技术总览 2017-03-10

PDF PDF 634 KB
New Modelithics COMPLETE Library Release v17.0 for ADS Represents over 15,000 Components 
Modelithics announces the latest release of the Modelithics COMPLETE Library version 17.0 for use with Advanced Design System (ADS) simulation software.

新闻资料 2017-02-15

 
Keysight EEsof EDA Premier Communications Design Software 
Keysight EEsof EDA premier communications design software product overview brochure.

手册 2017-01-24

PDF PDF 2.54 MB
M9421A VXT PXIe Vector Signal Transceiver - Data Sheet 
This configuration guide contains information to configure the M9421A VXT PXIe vector transceiver

产品资料 2017-01-18

PDF PDF 1.91 MB
Synthesis Made Easy With Keysight Genesys  
Learn how to quickly design many different RF circuits with various topologies in these short tutorial videos. These step-by-step tutorials walk you through the steps to accelerate your routine design tasks from hours to minutes with automatic RF circuit and system synthesis tools.

基本演示 2016-12-01

 
Integrating Multiple Technology Devices onto Laminate-Based Multi-Chip-Modules 
Microwave Product Digest (MPD) featured article on "Integrating Multiple Technology Devices onto Laminate-Based Multi-Chip-Modules Using an Integrated Design Flow", written by Keefe Bohanan, Applications Engineer District Manager for Keysight EEsof EDA.

文章 2016-11-29

PDF PDF 3.90 MB
Direct-Synthesis Software Approach Facilitates Filter Design 
This Microwaves & RF article discusses how Genesys software can be used to design filters with the direct-synthesis technique. A lowpass filter example is presented to illustrate the software’s capabilities.

文章 2016-11-28

 
Ericsson and Freiburg U. Design High-Q Power Harvesting Circuit Using ADS 
Keysight’s ADS harmonic balance was used to explore the design space around the innovative impedance transformation using a high Q quartz crystal resonator to transform the low voltage from the low impedance antenna to a voltage high enough to overcome the Schottky diode junction voltage.

案例分析 2016-10-19

PDF PDF 639 KB
The High-Frequency, High Speed Design Revolution: Why Your Design & Test Flow Will Soon Be Obsolete 
In this keynote from EDI CON USA 2016, Todd Cutler, vice president and general manager of Keysight Design & Test Software, discusses these trends and explains how, when coupled with market pressures, they are driving a revolution in the design and measurement industry.

基本演示 2016-10-11

 
Using DSP and RF circuit co-design to reduce risk and cost 
For modern design organizations, it’s now more imperative than ever that they simulate both Digital Signal Processor (DSP) and RF circuits together at the system level using mixed signals.

文章 2016-10-11

 
Software plus signal generators and analyzers support IEEE 802.11p design and test 
Jungik Suh, marketing program manager, Automotive & Energy Solutions, Keysight Technologies, provides input on several Keysight solutions for the connected-car arena for Evaluation Engineering's October print special report on automotive test.

文章 2016-10-05

 
Unlocking Millimeter Wave Insights 
It is easy to underestimate the challenges at millimeter-wave frequencies, and this amplifies the importance of integrated tools for design, simulation, measurement, and analysis. Learn more about how Keysight is taking the mystique out of millimeter waves and unlocking new insights.

基本演示 2016-09-30

 
Keysight to Demonstrate Latest Measurement, Design Innovations at European Microwave Week 
Keysight announces it will demonstrate a wide range of design, test and characterization solutions at European Microwave Week 2016, ExCel Exhibition Centre, Booth E2, London, Oct. 4-6.

新闻资料 2016-09-19

 
Getting Started with ADS 
In this short video, you will learn how to navigate through the ADS environment to create a new workspace, build a new schematic, and run a simulation.

基本演示 2016-09-11

 
How to Design Custom RF, Microwave and Analog Filters 
This video shows a custom filter design technique based on Direct or Exact Synthesis in which the filter response is first shaped and customized to meet specifications before a suitable topology is extracted and transformed for the most economical realization.

视频演示 2016-09-01

 

1 2 3 4 5 6 7 8 9 10 ... 下一页