検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

Metrology & Calibration Standards

Feel confident that Keysight metrology is behind every measurement you make

Measurement confidence

Know that every measurement is traceable to National Metrology Institutes (NMIs) through Keysight-engineered calibration procedures that verify instrument specifications.

Metrology advances

Rely on Keysight engineers who work with the NMIs to develop rigorous measurement techniques in existing and emerging technologies.

Shared expertise

Stay up-to-date on changing compliance requirements and their practical applications by working with Keysight metrologists who collaborate with international standards organizations.

YouTubeビデオを見る 

1-25 / 36

並べ替え
ATE System Level Calibration and Its Impact on Cost, Quality and Schedule - White Paper 
This paper proposes an alternative method to provide system level specification and system measurement calibration which will extend the system’s ability to be used for multiple products.

アプリケーション・ノート 2017-03-20

PDF PDF 651 KB
キーサイト標準ラボ校正 
デバイスの高確度を継続して保証

技術概要 2016-10-05

Calculating Measurement Uncertainty using Digital Multimeter Ratio Measurement Techniques 
This paper compares three DMM ratio measurement techniques for determining the traceable value and measurement uncertainty of an unknown input.

アプリケーション・ノート 2015-09-04

PDF PDF 761 KB
Using Calibration to Optimize Performance in Crucial Measurements - Application Note 
This application covers two goals: help you ensure that you get the calibration you expect (and deserve), and help you improve effective measurement performance through innovative use of calibration.

アプリケーション・ノート 2015-06-24

PDF PDF 1.14 MB
Calibration of a Ratio Transformer - White Paper 
Describes a calibration technique for decade ratio transformers which is performed by comparison measurement at 1kHz.

アプリケーション・ノート 2015-06-09

PDF PDF 735 KB
校正に影響を与える6つの要素 
校正サービスのサプライヤの選定は、非常に簡単なことだと思われています。なぜなら、校正という作業自体には大きな差はなく、認定サプライヤ(ISO9000登録やISO17025認定など)であればどのサービスやサプライヤを選択しても類似したサービスが提供されるはずだからです。ところが、実際にはそうではありません。校正には規制がないため、校正の成果物と価値には大きなばらつきがあるのです。

アプリケーション・ノート 2015-06-04

Specifications Guidelines - Technical Overview 
Keysight Technologies has definitions for its Test & Measurement product specifications and how they are presented. The following material is extracted from these manufacturing recommendations.

技術概要 2015-05-27

PDF PDF 245 KB
Connector Pin Recession and its Effect on Network Analyzer Accuracy - White Paper 
Outlines an experiment undertaken to assess the impact on the measurement of reflection coefficient when using 3.5 mm connectors.

アプリケーション・ノート 2015-05-20

PDF PDF 406 KB
Attenuation Measurement of Step Attenuators - Application Note 
Describes the T-matrix measurement method for achieving high accuracy in calibrating step attenuators.

アプリケーション・ノート 2015-05-20

PDF PDF 715 KB
Uncertainty Analysis for Uncorrelated Input Quantities - White Paper 
The Guide to the Expression of Uncertainty in Measurement (GUM) has been widely adopted in the different fields of the industry and science. Learn how to use for uncorrelated input quantities.

アプリケーション・ノート 2015-05-19

PDF PDF 502 KB
Revisiting Mismatch Uncertainty with the Rayleigh Distribution - White Paper 
This paper examines several important aspects of estimating mismatch uncertainty, which is often a major component of the total uncertainty for RF and microwave measurements.

アプリケーション・ノート 2015-05-19

PDF PDF 932 KB
Fully-Automatic DMM Calibration System - White Paper 
Describes a fully-automatic calibration system for digtial multimeters (DMMs), including the uncertainty estimation of DC Voltage measurements.

アプリケーション・ノート 2015-05-15

PDF PDF 1008 KB
A Guard-Band Strategy for Managing False-Accept Risk - White Paper 
Presents guard-band strategy for managing false-accept risk with only limited knowledge of the a priori probability that a device is in tolerance.

アプリケーション・ノート 2015-05-13

PDF PDF 260 KB
Defining Your Calibration Requirement - Technical Overview 
These are the steps that can be taken when actually placing an order to ensure you get a "proper" calibration.

技術概要 2015-05-12

PDF PDF 96 KB
Evaluation of the Performance of a State-of-the-Art Digital Multimeter - White Paper 
Describes several methods used to verify the performance of a very accurate automatically calibrated DMM, the HP 3458A.

アプリケーション・ノート 2015-05-07

PDF PDF 864 KB
Language of Specifications - Application Note 
This paper explains some of the arcane language used in describing a product's characteristics.

アプリケーション・ノート 2015-05-07

PDF PDF 695 KB
Selecting a Calibration Vendor - Application Note 
Cost is important but are there any other questions that need to be asked in selecting a calibration supplier?

アプリケーション・ノート 2015-05-07

The Metrological & Financial Implications of a Clogged Fan Filter - Application Note 
This article discussed the implications of having a clogged air filter and addresses solutions to helping in the prevention of clogged air filters.

アプリケーション・ノート 2015-05-07

Instrument Design Validation and Recommended Calibration Policy - Application Note 
Provides background information on the test philosophies and methods used when developing instrument verification and adjustment procedures.

アプリケーション・ノート 2015-05-07

Sensitivity Analysis of One-port Characterized Devices in Vector Network Analyzer Calibrations 
Results of a study on the use of characterized devices in microwave vector network analyzer (VNA) calibrations and measurements. A review of the theory of one-port characterized device calibration.

アプリケーション・ノート 2015-05-05

PDF PDF 290 KB
Establishing Traceability for Quantities Derived from Multiple Traceable Quantities - White Paper 
Provides method of developing traceability for measurements (eg. phase noise) that have no SI units.

アプリケーション・ノート 2015-05-05

PDF PDF 413 KB
Too Much Calibration? - White Paper 
This paper explains the variables at work in the world of calibration - how they can be used to find the elusive balance point between cost and confidence, or "too much" and "not enough" calibration.

アプリケーション・ノート 2015-05-05

PDF PDF 569 KB
Using a Manufacturer's Specification as a Type B Error Contribution - White Paper 
Examines the implications of using a manufacturer's specification in an uncertainty analysis; and how calibration laboratories use uncertainty data in their quality systems and customer-facing documents.

アプリケーション・ノート 2015-04-27

PDF PDF 1.03 MB
Isolating Frequency Measurement Error and Sourcing Frequency by Robert Leiby 
When performing a calibration, the risk of incorrectly declaring a device as in-tolerance (false-accept risk) is dependent upon several factors such as the specified tolerance limit and guard band.

アプリケーション・ノート 2015-04-27

PDF PDF 3.09 MB
Calibration Process Innovation Using Non-Required Guard Banded Testing by Richard Ogg 
Calibration services vary as to how to set the acceptance limits compared to the required tolerance. Using a guard band to reduce the acceptance limit will increase the confidence in the calibration.

アプリケーション・ノート 2015-04-24

PDF PDF 258 KB

1 2 次へ