Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Connected Car

The automotive industry is in the midst of a revolution that is gathering momentum as vehicles become the fusion point of innovative wireless and electronic technologies. Fundamental market forces such as safety, environment, security, and connectivity are accelerating the adoption of new technologies. This puts huge demands on OEMs, manufacturers and even chipset suppliers - to ensure reliability and quality. In order to meet the lofty goals of zero fatalities (or even zero accidents), enabling greener transport systems, and satisfying consumer demand for ubiquitous connectivity, the industry must continue to evolve and adapt quickly. The path to highly or fully autonomous vehicles will be challenging due to mission critical safety requirements of automotive systems, and the need for everything to reliably work in spite of interchangeable equipment from multiple vendors.

Keysight offers solutions to help you address these challenges in an ever changing environment.

1-2 of 2

Sort:
eCall/ERA-GLONASS Conformance Testing with Keysight E6950A - Application Note 
This application note discusses how designers can use the Keysight eCall test setup to emulate the various elements of a real eCall environment comprising GPS, automobile, cellular network and PSAP.

Application Note 2017-04-12

New Strategies for Managing Wireless System Complexities in the Connected Car - Application Note 
Application Note highlights several development challenges that arise from the implementation of complex vehicle wireless systems and how the automotive industry can easily adopt test methodologies used in new strategies for managing wireless system complexities in the connected car

Application Note 2016-11-15